Part Number: TLK10031 As per our requirement, our connection is as follows.
10G sfp signals from PORT_MAIN are connected to HS of TLK10031. LS signals of PORT_MAIN TLK10031 are connected to MUX, and can be switched to any of the devices( say LINK A, LINK…
Part Number: TLK10031 Hi,
My customer is interesting to TLK10031. The datasheet says this device support 10GBASE-KX. My customer want to know if it support 10GBASE-ER application?
Thank you!
John
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 , We have implemented the TLK10232 but use only one channel and want to replace it by the TLK10031.
As far as I have check, our design will be compatible with the TLK10031 except that the pin…
Part Number: TLK10031 Hi, as per our requirement, we want to use the Transciever TLK10031 without software provision? can we can able to handle via hardware alone? if any design document, please share us
Part Number: TLK10031 In the TLK10031 Pin Description table (Table 4-1), in the I/O Type column most or all of the LVCMOS outputs are described as "25 Ohm Driver", "40 Ohm Driver" etc. Does this refer to the resistive load that can…
Part Number: TLK10031 For the TLK10031 PHY can the following be confirmed?
For 1GBASE-KX (aka 1000BASE-KX) mode of operation:
Only Low Speed Interface signals INA0P/N and OUTA0P/N are required.
Low Speed Interface signals INA1P/N, INA2P/N, INA3P/N, OUTA1P…
Part Number: TLK10031 For the TLK10031 low and high speed interfaces, the layout guidelines (Chapter 10) in the datasheet state "Differential intra-pair skew needs to be minimized to within ±1 mil.". Does this rule take into account the…
Part Number: TLK10031 Hi Team.
I am using tlk10031.
High speed interface is XFI and low speed interface is AXUI.
However, PACKET LOSS occurs in the RX direction of the high speed interface. (HS_ERR_COUNT [15: 0] has been increased.)
We have reduced the…
Part Number: TLK10031 A few questions about TLK10031 JTAG:
For the end user, is the JTAG interface primarily for boundary scan (i.e. for production test)?
Does TI offer a USB-to-JTAG "pod" and software for a PC?
Is TLK10031 JTAG compatible…