Part Number: TLK10031 Hi
we are using TLK10031 device in our design. Our board is going for assembly in two weeks. Plz provide us the Reflow recommendations to be followed for this device.
Part Number: TLK10002FPGAEVM Hello,
maybe a silly question: The product page of the TLK10002 lists beside the evaluation board a FPGA board, that can be used as source to drive the TLK10002. The evaluation boards of the above mentioned TLK10022, TLK10031…
Hi,
Unfortunately, with further investigation this application TLK10031 will not work. When using SGMII there is no 8b/10b encoding of the data and the device will not be able to aggregate and serialize the data correctly. If you are able to use 8b…
Part Number: TLK10031 Tool/software: Linux Hello,
I am working on 10GE application. We were able to finish the prototype of the board.
In the FPGA, we have ZYNQ7000 connected to 10GE MAC IP, and this IP is connected to an external TI PHY through…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10022 , TLK10081 Hi,
The current application scenario is that the 4xSGMII interface of PowerPC is connected to the low-speed 4port of the TLK10031. Our goal is to connect the SFP+ through the high…
Hi Lucas, Thanks for this detailed answer. I appreciate it.
As I mentioned, I'm trying to interface the 10GBASE-KR interface from a CPU to a 10GBASE-SR optical SFP+ transceiver. Regarding the TLK10031, I think its XAUI interface is used to interface…
Part Number: TLK10031 Hi,
we have an FPGA-based measurement system. I can implement a 4-lane JESD204B interface (one way, transmit from FPGA) at up to
3.125Gbit/s per lane on that FPGA. I want to combine these lanes and send the data via an SFP 10Gb optical…
Part Number: TLK10031 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Is TLK10031 IBIS model available or TLK10032 (Dual Channel version) IBIS model Channel A needs to be used ?
Part Number: TLK10031
Hi,
We designed a custom board connecting the TLK10031 PHY to a Zync FPGA. We are going to use it in the 10GBASE-SR configuration but currently we don't have any input SFP+ signals (HS) connected. We developed and verified 10G MAC…