Part Number: TLK10031 Other Parts Discussed in Thread: TLK10034
Hi,
Once link training has completed, the 10G-KR data path is enable but the link is lost on one of the test boards when the power supply is turned on and off repeatedly. Looking at the difference…
Part Number: TLK10031 Hi,
For LS_EQ[3:0] register, there is mentioned on page 66 of TLK10031 data sheet, but the detailed feature isn't mentioned. So, could you please provide the information in detail such as the following HS_EQREF[2:0] register …
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232
Our setup for the TLK10031 is:
- HS side: connected using SFP+ optical connector to the SFP+ of another PCI card connected to a PC at 10G rate.
- LS side: connected to 4 channels XAUI for…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10034 Hi,
For HS_EQPRE[2:0] register, there is mentioned on page 60 of TLK10031 data sheet, but the detailed feature isn't mentioned. So, could you please provide the information in detail …
Other Parts Discussed in Thread: TLK10031 , DP83869 Tool/software: Linux Hi Team,
The TLK10031 also supports 1G (1.25 Gbps) mode. Could you tell me how to configure this pattern? Thanks.
Sincerely,
Part Number: TLK10031 Hello! Our current design is to use the powerPC MDIO interface to control the TLK10031, using the clause45 mode. After the first addressing, the powerPC queries the mdio interface ready and sends a reading command. From the oscilloscope…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 Hi team,
Let me confirm the datasheet value.
I saw the following value from TLK10031 datasheet P.57. Is this value right?
1 = Selects REFCLK_0 P/N as clock reference to HS side serdes macro…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 ,
Looking at the datasheet of the TLK10031 and TLK10232, it seems that they both have the same power consumption.
But the TLK10031 is single port and the 232 is dual port, so it doesn’t make…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 Hi,
Our system setup with the TLK10031 as shown below.
We want to operate TLK10031 at 10GBASE-KR mode. No optical module/cable.
The following is what I tried;
On FPGA side, loopback…
Part Number: TLK10031 Hello,
We are using the TLK10031 to convert from XAUI to 10GBASE-KR. The below figure shows the data flow path in our design:
SWITCH <-------------> TLK10031(LS)<------------>TLK10031(HS) <------------> SFP+
XAUI …