Part Number: TLK10232 Other Parts Discussed in Thread: DP83869 I need to implement a bridge between PCIe and 1000BASE-KX. Does TI support this with a PHY or similar? If not is there an alternate solution like PCIe to XAUI etc. and a secondary device to…
Part Number: TLK10232 Other Parts Discussed in Thread: DS100BR111 Is there any product which will support as Retimer/ Redriver or just as transceiver for dual channel 1000BASE-KX to backplane ethernet i n a small package.
Regards,
SP
Part Number: TLK10232 Hi,
Looking at SPRA953C and the TLK10232 datasheet, equation 5 requires RΘJC for the calculation.
Table 10-1. Package Thermal Characteristics
JEDEC STANDARD BOARD
PARAMETER
VALUE
ΘJA
Theta-JA
25.5
…
Part Number: TLK10232 Hi,
The 10232 datasheet states the OP temperature as -40°C to +85°C free air operating and maximum junction temperature of +105°C. What are the Theta-JC and Theta-JA for the package? Also, will heatsinking the package enable operation…
Part Number: TLK10232
Hello, We have used TLK10232 dual phy component for a XAUI to SFP/SFP+ application.
I have a question regarding the value of HS SERDES multiplier setting (Reg 0x1e.0x0002.[3:0])
We operate the chip at REFCLK frequency set to 156.25MHz…
Part Number: TLK10232 Hello, We have used TLK10232 dual phy device for a XAUI to SFP/SFP+ application and we have a problem in 1G link establishment when auto-negotiation is enabled.
The initialization of the device is shown below:
Reset device (assert…
Part Number: TLK10232 I am using the TLK10232 in one of our designs. The TI website has Mentor Graphics decals for the device. Unfortunately, they do not import into my version of Mentor Graphics VX.2.8 with integrated library. What I need is a drawing…
Part Number: TLK10232
Hello,
We are facing optical bit errors with new SFP+ modules combined with a TLK10232 in a proven system. 1000+ units built and running.
When using a more recent SFP+ module, link errors increase (from BER test >10^12 downto…
Part Number: TLK10232 Hi ,
We have two SFP+ which is connected to HS* pins, One (portA) SFP+ is working fine another one (port B) has errors and channels are very short which is within 2inch.
Please let me know if any easy method of tuning the equalizer…