Part Number: TLK10232 I'm trying to figure out how to interface the low speed side of the TLK10xxx family (specifically the TLK10232) to normal FPGA IOs (specifically to a Xilinx Artix FPGA) for data rates up to 1.25Gb/s per lane on the low speed…
Part Number: TLK10232 Hi,
when I use TLK10232 at 10GKR mode, I use tester insert CV error. I check counter 0x10. it max value is 0xFF. Why it is not 0xffff? Do I need setup more?
Dump FPGA MDIO group 3 phy 06 dev 1e 00: 0610 0B26 8316 A848 1500 2000 F115…
Part Number: TLK10232 Hi,
if I want to use 10.3125G at TLK10232, could I use general purpose mode?
if it must run at 10G-KR, does it must use clause 45 mode?
Thanks
Part Number: TLK10232 Hi,
when I use TLK10232 at 10GKR mode, I use tester insert CV error. I check counter 0x10. it max value is 0xFF. Why it is not 0xffff? Do I need setup more?
Dump FPGA MDIO group 3 phy 06 dev 1e 00: 0610 0B26 8316 A848 1500 2000…
Part Number: TLK10232 Other Parts Discussed in Thread: DS125DF1610
When I use PRBS at TLK10232, do I need set PRBSEN pin to high? Or, I just set reg:0x0b tx, rx and patten.
when I send pattern through DS125DF1610 cross back to TLK10232. reg:F will sometime…
Part Number: DP83869HM Other Parts Discussed in Thread: TLK10232 , DP83869 Hello,
We are considering the following design approach for i.MX8MP to work for a 1000Base-kx.
This approach involves two ICs. The first IC (PN: DP83869HM) is tasked with converting…
Part Number: TLK10232 We have a module Testcard which employed TLK10232 for manufacture line test purpose. In the recent build of this card, we found 15 out of 80 cards be failure (failure rate almost 20%).
On the failure cards, we measured that the…