Other Parts Discussed in Thread: TLK10232EVM Hello. Is there a Capture schematic of the TLK10232EVM available? I see the pdf version online but I would like to have the schematic in its native format.
Other Parts Discussed in Thread: TLK10232 , CDCM6208 Hi.
After power is applied to the EVB , (TEST Pattern (PRBS) Generation, TEST Pattern (PRBS) Generation function ) BER tests on the steps (procedures) in sequence , tell us , testing in progress , which would…
Other Parts Discussed in Thread: TLK10232EVM HI. I'm Carl.
My customer has question about tlk10232evm question.
After power on the EVM Board, tell me to order the procedure for carrying out the test of TEST Pattern(PRBS) Generation, TEST Pattern(PRBS…
Other Parts Discussed in Thread: TLK10232 Dear TI team,
This is Matthew.
I’d like to control TLK10232 EVM using our’s system GUI . (Now , I control TKL10232 EVM using TI GUI.)
To do that, I have to merge the control GUI of TLK10232 with Our…
Hi Daniel,
Thanks for the block diagrams with various test cases. Can you confirm that the signal flow I annotated on the FPGA is correct? I have also numbed the test cases for ease of discussion.
I have a couple of questions related to your setup.
…
Hi,
Related to: " The evaluation boards of the above mentioned TLK10022 , TLK10031 or TLK10081 look very similar, but the FPGA board is not listed there. Nevertheless, would it be possible to use the TLK10002FPGAEVM as a companion to TLK10022EVM or…
Hi,
I tried your procedure. However, HS error has occured one of TLK10232EVM board again. I performed your procedure after GUI opened.Then, leave 12 hours and read CHANNEL_STATUS_1 and HS_ERROR_COUNTER.
CHANNEL_STATUS_1 HS_ERROR_COUNTER TLK10232EVM Board…
Kai,
The test was very simple. I measured the DC resistance as seen across the RX diff pair using a multi-meter.
Power up TLK10232EVM.
Ensure receiver termination is enabled through HS_ENRX bit field.
Measure the RX termination with multi-meter via the…
Hi Eli,
How many lanes are you planning to use? This device accepts 8b/10b coding. In 10G General Purpose mode the maximum line rate in the high speed side is 9830.4Mbps @122.88/153.6MHz.
The TLK10031 is pin to pin compatible, since this device is just…
Hi Kanemaru,
LS_OK_IN_A should be pulled-up through a 49.9K resistor to VDDO. Even, you could take the TLK10232EVM as a reference design.
Regards,
Luis