Hello Gerald,
Thanks for the update. Going through our catalog, it seems the best solution would still be the SN65LV1023A/1224B for the CY7C9689. TI doesn't have devices that have 4B/5B or 5B/6B coding schemes.
For the CY7B933/23, similar to Atul…
Other Parts Discussed in Thread: TLK3132 , TLK6002 Hi,Team,
I have some quesitons about the two serdes parts. Need you help.
1)Can TLK3132 work in different datarate for two channels?
2)Can TLK3132 support different datarate for Tx and Rx in same channel…
Other Parts Discussed in Thread: TLK3132 In my design I use the TLK3132 device and I have the following situation:
I have external H/W loop and the Self Test is working properly.
Then I de-activate the internal Self Test and I send a specific pattern…
Other Parts Discussed in Thread: TLK3132 Hi,
In developing PCI Express based Network interface card, one is using TLK3132 for SERDES to GMII conversion for packet processing between MAC and PHY with help of FPGA's.
So, how the Auto-negotiation stuff…
Other Parts Discussed in Thread: TLK3132 Hi,
I would like to use tlk3132 in TBI mode where in serial data will be in SGMII
mode and these needs to be convert to TBI and another side I am planning to
use another TLK3132 to convert the given TBI to SGMII…
Other Parts Discussed in Thread: TLK3132
Gilbert,
The answers are listed below.
-Atul
H ello,
One of my customers is developing with our TLK3132 :
They
have some questions…
Other Parts Discussed in Thread: TLK3132 Hi and good morning.
I’m not sure if you’re also supporting the Ethernet Transceiver Products.
The question is to interface a Avago SGMII Transceiver with a FPGA with (R)GMII- Interface only.
I’ve found…
Other Parts Discussed in Thread: TLK3132 , TLK10002 , TLK6002 , TLK3131 , TLK3134 , DS32ELX0421 , DS32ELX0124 Hi Team,
Is there a TI SERDES device that can provide 3Gbps data without using an encoding scheme?
Customer is looking at bringing parallel data out…