Hi Sir,
We designed and Simulated the 0-20mA current transmission using XTR111 and Verified the Results also...This circuit we are placing as a Alternate circuit for V-I Converter discrete design (Discussed in previous message).
1) So can you please verify…
Hi Ronald,
1. I want to increase the gain maximum of 5. How to increase the gain ?
2. Yes. Sine quality can be ignored. The output of TLV172 (VOUT) is uni directional signal (pulsated) and I want to convert it into pure DC signal for feeding as analog…
Part Number: TLV6001 Other Parts Discussed in Thread: OPA172 , TLV172 , TLV9351 , OPA990 , LPV511 Sir/Madam,
Can we connect +5V at V+ and -5V at V- as input power supply to TLV6001IDCKR?
Got this confusion as page 9 , under section 7 is mentioned as : VS= 1…
Part Number: TLV2172 Other Parts Discussed in Thread: TINA-TI , TLV172 Tool/software: TINA-TI or Spice Models Hi
I download TLV172.TSM from the web and use it.
When the TLV172 is operated with a voltage follower,
the power supply voltage is ± 8 V, and when…
Hi,
thank you for your answer.
TINA-TI is installed in the following folder.
C:\Program Files (x86)\DesignSoft\Tina 9 - TI
1. Download the sboma.tsc file in the following folder Is it ok?
C:\Program Files (x86)\DesignSoft\Tina 9 - TI\EXAMPLES\TI Test…
Part Number: NE555 Other Parts Discussed in Thread: CD4017B , TLC555 , TLV172 , LM358 , LF347 , LF353 I read somewhere that a single NE555 would not be able to create a biphasic square wave, only monophasic. I am wondering whether that is possible. If not…
Hi Kai,
You mean TLV172? not TLV712?
I used THS4521 to amplify the output voltage of 2.05V from AMC1301 and to achieve differential voltage signal too.
For the datasheet of TLV172, in section 7.7, which parameters should i take note of? I am not good…
Part Number: LM2776 Other Parts Discussed in Thread: TLV172 , TPS60400 With LM2776 I want to feed the negative supply of two TLV172 from +3.3V. If 3.3V is fast rising everything works well but at slow rising supply the LM2776 starts too late and the current…