Other Parts Discussed in Thread: TLV320AIC10 Hi,
Iam working on integrating TLV320AIC10 codec with AMBE2000 vocoder. I have configured TLV320AIC10 to work at SCLK of 2.048 MHz, FS is 8kHz. Input is selected as AURXM and AURXFP through configuration. For…
Other Parts Discussed in Thread: TLV320AIC10 I am looking at using the TI TLV320AIC10 as an SPI slave to my microcontroller. I have the following two questions of which the data sheet does not provide an answer. The data sheet for the TLV320AIC10 states…
Hi all,
I have previously installed two AIC11 codec in my EVM and now remaining six with AIC10.
AIC11 DVDD1 operates on 1.1V-3.6v where as AIC 10 DVDD
is 3V-5.5V
My question is that can i cascade and operate both the ICs ie AIC10(U1 and U2) and…
Part Number: AM1707 Other Parts Discussed in Thread: TLV320AIC10 Hi Team,
I have a customer with some questions about the AM1707:
1. We have CF card in the design, but in AM1707 there is only MMC/SD card support. What should be done to use CF card?
2…
If I use an external 12.288MHz oscillator for the MCLK on the AIC3254 will I still get my 48KHz sample rate?
Also Is there a Master/Slave mode on the AIC3254 as there was with the AIC10?
The eval boards all show the USB chip providing the clock, I am…
Part Number: TLV320AIC1110 Other Parts Discussed in Thread: TLV320AIC10 Do i need to configure only through I2c interface or can i configure it by SPI interface. How do i configure ? Using which software? Do i need to write code ? From where i need to…
Other Parts Discussed in Thread: TLV320AIC10 Hi,
Is there any reference design connecting McBSP with Codec. We need to connect F8069 with TLV320AIC10 codec through McBSP. It will be helpful if there is a reference guide or schematics.
Best Regards Kummi