Hi,
We are using TLV320AIC14k in our custom design. We are using master slave cascade configuration. We want to use this in turbo mode.
The figure in attached file (asp.bmp) shows the cascaded configuration.
CODEC1 is master.
CODEC2 is Slave…
Other Parts Discussed in Thread: TLV320AIC12K Hi,
I'm working on a new design with the TLV320AIC12K CODEC, and am trying to figure out how the thermal pad on the QFN (AHB) package should be connected. The datasheet (Jan 2007 revision: http://focus…
Hi,
Thinks, I just test Register 4, this way, I send 0x04 as register address, send 0x1A as data. When reading, I can only read the value 0x30 ,which is the default data.
I do some search in the community, and I find someone had same problem with me…
Hello Luis Fernando,
Due to the footprint, I changed to TLV320AIC12K, which is supposed to be the same but adding analogue outputs.
Since the datasheet of both of them is the same document, I assume that TLV32012K digital output is also 2's compliment…
Hi
I have purchased the tlv320aic12k /14k DBT_EVMB. I have installed the software to run it but only the driver software doesn't get installed. Any idea as to why is doesn't?
Other Parts Discussed in Thread: OMAPL138 , TLV320AIC12K Hi,
We are in the design phase of a handheld device with OMAP L138.
We are planning to derive an FPGA and …
Other Parts Discussed in Thread: TLV320AIC14K I use the TLV320AIC14K output in single-ended mode (OUTP1) with 2uF DC-decoupling and a load of 10kOhm (OUTM1 unconnected).
Vcc = 3,3V; Samplingrate = 22,05kHz, fullscale sinus 1000Hz, outputamplifier 0dB …