Part Number: TLV7211 Other Parts Discussed in Thread: LMV721 hi all,请教个问题: ant _stimulation_1116 - 副本.TSC
使用LMV721搭建一个电路检测电路,实现当输出电压值Vout大于三极管T1的基极导通电压后,三极管T1导通,将Vout拉低,即VF1输出低电平,但实际仿真结果不符合预期,请问大家有什么建议
Part Number: LMV721 hi all,请教个问题: 1832.ant _stimulation_1116 - 副本.TSC
使用LMV721搭建一个电路检测电路,实现当输出电压值Vout大于三极管T1的基极导通电压后,三极管T1导通,将Vout拉低,即VF1输出低电平,但实际仿真结果不符合预期,请问大家有什么建议
Part Number: TLV7211A Other Parts Discussed in Thread: TLV7211 Hi team
The customer uses TLV7211 to design comparative circuits, and this project has been mass-produced multiple times. However, using the latest batch of TLV7211 (2422+5) will result…
Part Number: MAX232 Other Parts Discussed in Thread: TLV7211 , LM2765 Ich benötige in einer Schaltung nur die positive Spannung vom MAX232
Über die Kondensatgoren C2 und C4 wird die Negative Spannung erzeugt.
Wenn ich jetzt die Konsdensatoren weglassen…
Part Number: TLV1811 Other Parts Discussed in Thread: TLV7211 , LMC7211 Tool/software: Dear TI expert,
I'm testing the component in the simple configuration and not able to work. I don't know what is the problem.
Tested on bare PCB with no other…
Part Number: CD4050B Other Parts Discussed in Thread: TLV1811 , TLV7211 , UCC27527
Hi Clemens
Thanks for your prompt support in the past.
I've a few supplementary Q's, answers to which I could not gather from the Data Sheets.
Pl be good enough…
Part Number: TLV2381 Other Parts Discussed in Thread: LMC7211-N , TLV7211 , TLV3701 , TLV1811 Hi,
I want to measure the quiescent current of TLV2381IDBVRG4. Could you please help me with the test set up?
PLease have a look on my schematic
…
Other Parts Discussed in Thread: TLV7211 , LM393 , CD40109B Hi,
In my application, I need a falling edge detector that can take high-voltage inputs (up to about 12 V or so). Therefore, I'm looking into using TLV7211 as the comparator of choice. This…
Other Parts Discussed in Thread: LMC7101 , LMC7211 , LMC7225 , TLV7211 , LMC7215 , LMC7221 Hi Team,
Our customer is looking for the comparator with SC-70 package and below pin-outs, can you help to check if we have such device? Thanks a lot!
Other Parts Discussed in Thread: TLV7211 , TLV1805 Hi team,
I am looking for an IC which can convert digital 0/1 signals to 7V/-0.4V logics/pulses. Could you please recommend one for me?
Thanks very much!
Bruce