Part Number: TLV741P Other Parts Discussed in Thread: TLV713P , Hi,
1. What is the difference between TLV713P and TLV741P?
2. Which one is the most recommend.
Thank you.
C.T.
Part Number: TLV741P Hi,
Would it be safe placing af 220uF even though it is not within the range in the data sheet (i.e. min. 1uF, max 100uF)? What is the maximum capacity for garenteed stable operation?
Regards,
Peter
Part Number: TLV741P Other Parts Discussed in Thread: TLV757P Dear Specialists,
My customer is considering TLV741P and TLV757.
I would grateful if you could advise about his question.
---
Where should be connected to GND or floating.
According to the…
As you have seen, that power supply circuit has bad load regulation. Consider using an integrated regulator like the TLV741P or TLV713P.
Different logic families have different power consumption. But a weaker family like HC might not be able to drive…
Part Number: SN74AXC1T45 Other Parts Discussed in Thread: TLV741P , TLV740P For the low side VCC input, can we take the high side supply and use a voltage divider to support power to low side VCC?
Is there any concerns on noise or voltage variation?
Hi Yu-Chen,
Thanks for sending this over. I would actually recommend the TLV741P here. Specifically TLV74133PDBVR should be pin-to-pin solution. I will go ahead and make sure these are added to cross reference tool.
regards,
Wilson
Part Number: TPSM82822 Other Parts Discussed in Thread: TPS62864 , TPS62088 , DAC53608 , DAC121C081 , TLV741P , TPS7A10 , TPS74701 , TPS7A11 , TPS7A02 Hi,
We have identified TPSM82822 to use in our design.
The output voltage should be software controllable with…
Part Number: TPS7A25 Other Parts Discussed in Thread: TLV741P Hi TI,
1.) I would like to know can TI provide Output current limit graph like below for TPS7A25?
Below graph are taken from TLV741P datasheet
2.) The Output current limit written in datasheet…
Hi Mike,
For LDOs please look at the following devices for wearable applications:
TLV741P, TPS7A05, LP5907, or TPS7A10 (needs bias rail)
TLV741P, TPS7A05 and LP5907 are in 1x1 packages
TPS7A05, LP5907 and TPS7A10 are in WCSP packages
Best Regards,
Wi…