Part Number: TM4C123FH6PM
Hello.
Q1> I cannot jump from Main () to ISR(ButtonKeyIntHandler) when the PA [2] through PA[5] button is pressed.
Please explain what is wrong
Best Regards,
Jame,Shin
ButtonKeyIntHandler ( )
{
uint32_t ui32Ints;
ui32Ints…
Part Number: TM4C123FH6PM Other Parts Discussed in Thread: AM1802 Tool/software: Code Composer Studio I want the XDS200 debug probe work with CCS version 9.3.0.
The issue:
Using CCS 9.3.0.00012 I try to load my project using debug and I get this warning…
Part Number: TM4C123FH6PM
Tool/software: TI C/C++ Compiler
Hello!
Developing custom boot loader for our project I need to place it's code to special place in FLASH, so it will not erase itself and configuration data during firmware update. This bootloader…
Part Number: TM4C123FH6PM
Tool/software: TI C/C++ Compiler
Hello!
I have the following code in my project:
const uint8_t A3InitSub[] =
{
SQ_CFLOAT(5000 * 4),
SQ_CHW(2, 2), // Freq
SQ_CFLOAT(2000 * 4),
SQ_CHW(2, 3), …
Part Number: TM4C123FH6PM Hello!
My design contains special jumper to set up firmvare update by entering boot loader. here is the schematic part:
The line BOOT/EXT_RST is multiplexed with reset for LCD. Measuring on pin 10 of CPU I see high level then…
Part Number: TM4C123FH6PM
Tool/software: TI C/C++ Compiler
Hello!
Due to nature of application I am creating some objects with new operator during ISR (usually it is event objects with some extra data), and sometimes I create and delete objects in main…
Part Number: TM4C123FH6PM Tool/software: Code Composer Studio Hello Everyone, After flashing a program that went to Fault ISR, I no longer can connect to the chip I have.(TM4C123FH6PM) I get flashing Red Light on the probe and you may find the log files…
Part Number: TM4C123FH6PM Other Parts Discussed in Thread: EK-TM4C1294XL , , TPD4S012 , EK-TM4C123GXL
Tool/software: Code Composer Studio
Hello Everyone,
I am having trouble on the msc application on my custom pcb. I first developed an application to read…
Part Number: TM4C123FH6PM Tool/software: Code Composer Studio Good day!
Recently I realized that USB library has small error:
//*****************************************************************************
//
// USB_CDC_SET_CONTROL_LINE_STATE, wValue…