Part Number: TMDS181 Dear Sir,
I found some topic about this, the TI fae told the TMDS181 only support dc-coupled input, doesnt support ac-coupled input!
In fact ,the TMDS 181 function diagram , there are pull-up resisters (50 ohm) connected with Vbias…
Part Number: TMDS181 Tool/software: Hi team,
Is it able to use Script mode of Eyescan tool to generate Rx status (such as TMDS clock) output in real-time?
Customer wants monitor the device operating status in real-tim.
REgards,
Hayashi
Part Number: TMDS181 Tool/software: Hi team,
I saw the users guide of TMDS181 (sllu228a): https://www.ti.com/lit/ug/sllu228a/sllu228a.pdf
There is a description below. Have this bug fixed in new GUI already?
Regards,
Hayashi
chiu wesley said: FPGA input requires to be AC coupled, but TMDS181 output needs to be 3.3V common mode voltage, so use external 50ohm termination to 3.3V to set the CM. But 50ohm termination and FGPA input termination create double termination so output…
Part Number: TMDS181 Hello,
I have developed HDMI in interface to Zynq ultrascale+ FPGA through TMDS181 chip.
It does not share EDID information. Source is a Laptop. When we probe DDC signals they keep remain high all the time when HDMI cable is connected…
Part Number: TMDS181 Other Parts Discussed in Thread: TUSB3410 Hi team, I'd like to connect the TMDS181 to TUSB3410 for eyescan tool. Another thread said that we need to use firmware for TUSB3410. https://e2e.ti.com/support/interface-group/interface…
Part Number: SN65DP159 Other Parts Discussed in Thread: TMDS181 HI Ti TEAM:
We want to use SN65DP159 at the HDMI 2.0 RX side to replace TMDS181.(We want to remove TMDS181)
HDMI CONN(HDMI 2.0 RX) ---> SN65DP159--> Xilinx FPGA --> (XILINX HDMI IP)…
Hello, Jeevan,
You can check that there good isolation on your HPD pin from any of your power planes or pins.
What you are seeing is not expected since expected behavior is as follows:
Without any device connected to J28:
HPD_SRC measures 0 V
HPD_SNK…
Part Number: TMDS181 Hi team,
Customer want a device that can support all HDMI input resolutions in the list. I'm not sure if TMDS181 can work here. If not, could you pls help to pick out which resolutionTMDS181 isn't able to support? And do you have…