Part Number: TMDS181 Hi team,
Customer want a device that can support all HMDI input resolutions in the list. I'm not sure if TMDS can work here. If not, could you pls help to pick out which resolution TMDS181 isn't able to support? And do you have…
Part Number: TMDS181 Other Parts Discussed in Thread: SN65DP159 , TDP1204 , TMDS1204
Hi,
1. Customer wants to use TMDS181 as input side (source). The TMDS181 receives AC-coupled signals, but could you please tell me a reference circuit or precautions for…
Hello, Einav,
Is there a reason that you are not considering the use of TMDS171 instead?
The TMDS171 is a 3.4-Gbps HDMI 1.4b TMDS retimer.
Thanks,
Zach
Part Number: TMDS181 Hi Team,
TMDS181 is used in our product.
The ACTIVE DDC BLOCK wants to be set to the snoop option.
SCL_SNK/SDA_SNK is connected to the DDC of SRC and SNK to implement the snoop function.
Do I understand it correctly?
What is the purpose…
Part Number: HD3SS215 Other Parts Discussed in Thread: TMDS181 If the HD3SS215 is used to feed one sink from two sources but I place a TMDS181 in front on both inputs. Would this still be considered as a sink side termination? Meaning, place 47k pull…
Part Number: TMDS181 Dears
For the SDA_SNK pin in TMDS181, I want the details i.e., allowable undershoot, overshoot voltages and the duration of those. I saw the datasheet. So, typically, I know that the maximum is 6 V and the minimum is -0.3 V. I want…
Part Number: TMDS181 Other Parts Discussed in Thread: SN65DP159 Hi,
The datasheet says the following: "During the clock frequency detection period and the retimer acquisition period that last approximately 7 ms, the TMDS drivers can be kept active (default…
Part Number: TMDS181 Hello,
According to datasheet A1 contains internal Pull Down. Is the state of A0 (pin21) defined when left floating please?
BTW: TMDS181 eval board is responding on 5E address when these pins are left floating.
Thank you.
Hello, Jeevan,
Jeevan Sidharth G said: The Design in the pdf that I had attached in the beginning worked with FB36 being DNP.
Could you clarify what you mean by this? I understood that you were not getting a HPD signal to the source.
Thanks,
Zach