Part Number: TMDSDSK6416 I have configured MCBSP to work as UART using technical reference spra633c. I am using a scenario in which two DSPs communicate with each other over UART. This UART configuration works fine when tested with TTL or any other microcontroller…
Part Number: TMDSDSK6416 I am trying to use DSP/BIOS on TMSDSK6416 with CCS compiler version v6.1.3. I have installed the following products:
1) DSP/BIOS version v6
2) xdcTools version 3.3
3) SYS/BIOS version 6.46
I am added the environment variables…
Part Number: TMDSDSK6416
Tool/software: Code Composer Studio
good day. Currently, I have the TMS320C6416 DSP Starter Kit (DSK) . A bit old but quite powerful card. As a complement to this test hardware I am using the book:
Digital Signal Processing and Applications…
Part Number: TMDSDSK6416TMDSDSK6416 input is 5V. But 3.3 V output is not coming. Moreover U7 and CT4 is producing heat. The output at CT4 is coming 0.1 V instead of 3.3 V.
Kindly suggest how to resolve this issue related to hardware.
Part Number: TMDSDSK6416 I was initially tested TMS320C6416 based DSP Starter kit with the 6416DSK Diagnostics test with windows 8 PC it was successfully detected the board. Now again I am trying to do the same test with windows 8 and windows 10 based…
Part Number: TMDSDSK6416
Hello,
I'm trying generate short pulses with DSP's 32-bit timer. I'm using the DSK6416 board. I need to have pulse widths as short as 50ns-100ns and be able to change the duty-cycle. I try to read the CNT register of the timer…
Part Number: TMDSDSK6416 I need a daughter card for the TMDSDSK6416 so I can have a RS-232 communication link to it.
Our website shows the following cards, but it seems the company is no longer in service. Do you have any alternatives for these products…
Part Number: TMDSDSK6416
Tool/software: Code Composer Studio
Hello All,
I Started working on DSK6416 ,and followed a book by Rulph Chasing ,which has lot of examples to get start with DSK.
Well the book uses CCsv3.1 for compling and debugging the examples…