Part Number: TMDSDSK6713
Many times a code line is seen in programs related to aic23 codec
The line is as follow:
DSK6713_AIC23_CodecHandle hCodec;
What is it?
Is it a variable or a function?
and What is meant by codec handle and hcodec here?
Part Number: TMDSDSK6713
I am trying to use the example code from SPRA633. My working set consists of:
DSK6713 evaluation board
Code Composer Studio V10. With the .default DSK6713 gel file, supposed to run the DSP at 225 MHz)
Blackhawk USB560v2 emula…
Part Number: TMDSDSK6713 I made a small test program to check the functionality of the EDMA data transfer when the MCBSP triggers a REVT event. I achieved to receive an interrupt when EDMA completes data transfer to the receive buffer. However, this only…
Part Number: TMDSDSK6713 While using the Google search about programming of 6713 dsk through code composer studio. I came across multiple header files especially ''csl.h '' and "ledcfg.h'
?
What are the application scenarios of…
Part Number: TMDSDSK6713 When TI releases DSP KIT 6713, at that time version of CCS was 3,but now there are later versions available also.
The issue with ver 3 of CCS is that can only run on windows xp.
So my question is that can we use dsp kit 6713…
Part Number: TMDSDSK6713
Hi Team,
Our customer is requesting for the schematic diagram, reference manual and user's guide of TMDSDSK6713. I have search the forum but I can't find these documents. Can you please share a copy?
Regards,
Danilo
Part Number: TMDSDSK6713 Is it possible to use and program DSP kit c6713 through python? If yes ,how?Please kindly guide,through which version of python and how?
Part Number: TMDSDSK6713 Tool/software: Code Composer Studio I am using windows 10 and i want to use and program dsp kit6713, but what i heard is that this kit is only compatible with ver 3 of ccs,but ver 3 of ccs can't run on windows 10. How i can solve…
Part Number: TMDSDSK6713 Dear all,
we are using TMS320C6713 DSK Board with CCS V6 when tried to connect with CCS but its giving emulation error, debug is not happening and all the LED (including Busy LED) will be switch ON once power is connected is the…
Part Number: TMDSDSK6713 Tool/software: Code Composer Studio Dear Forum
Time ago I was using the DSK6713 ,with a older version of CCS .
I have also the Blackhawk USB560M ,14 PIN Jtag Emulator
Is my intention to develop new project on the TMS320 C6713…