The series resistors are likely used for helping with any possible signal integrity issues. A series resistor is often placed near the driver/source to help match the output impedance of the driver with the PCB to minimize any signal integrity issues…
Part Number: TMDSIDK574 I test TMDSIDK574 giga ethernet performance by iperf3.
One TMDSIDK574 is setting iperf server, another TMDSIDK574 is setting iperf client.
Test CMD:
Server: # iperf3 -s
Client: # iperf3 -c 192.168.2.249 -t inf
The bitrate is around…
Part Number: TMDSIDK574 Hello Dear TI Team,
I bought the TMDSIDK574 kit. I couldn't install RTOS SDK on this kit.
I connected the TMDSIDK574 kit to a display via HDMI. There are also two SD cards included in the kit. It says 'Industrial SDK' and 'Linux…
Part Number: TMDSIDK574 Hello Dear TI Team,
I want to control AC servo driver with EtherCAT communication protocol. I bought for this project TMDSIDK574 development kit.
But, I need help developing the software with this development kit.
Sinan, Thanks and…
sun ruijie said: i have knew the board info is like this, but i have some errors to burn the board information to emmc,
I checked with the author of the patch & we have not tried burning the eMMC pre-production. It will be helpful if you could answer the…
abc said: CortexA15_0: File Loader: Verification failed: Values at address 0x00000020 do not match Please verify target memory and memory map. CortexA15_0: GEL: File: C:\Users\abc\workspace_v12\helloworld\Debug\helloworld.out: a data verification error…
Part Number: TMDSIDK574 Hi there.
Does TI support EtherCAT slave implementation with PRUICSS under Linux?
I just found slave implementation document on TI RTOS but not on Linux.
Any link on relative document would be helpful.
Thank you.
Part Number: TMDSIDK574 Other Parts Discussed in Thread: AM5749 Dear Expert Team
We are trying to use McSPI peripherals on AM5749 on the custom board. Firstly we tried to test McSPIs on idkAM57x board.
After building and run the McSPI sample code, McSPI3…
Part Number: TMDSIDK574 Hello
I use TMDSIDK574, CCS11, OS is Kubuntu 21 with kernel 5.13.0-20.
I try connect to the board using embedded usb XDS100v2 debug probe and every time it fails.
Error code is:
The value is '-604' (0xfffffda4). The title…
Part Number: TMDSIDK574 Dear TI,
From the follwing patch,the am57xx supports that read board id information from the emmc boot1 partition,
I'm curious how to put the information in emmc, is it convenient to tell, because our customer's board does not…