Hi Daniel,
Daniel Kakaley said: I was hoping that you would leave the user's guide as is, and update the layout of the HDK so that it meets the definition in the Users guide. This would allow the HDK user to prototype with additional peripherals such…
Part Number: TMDX570LC43HDK Hi ,
I bought 4 nos of TMDX570LC43HDK and out of three are defective.
1.Heating of Ic and stopped working.
2.Unbale to flash the code
3.Board are not working.
After removing the following code from HL_sys_core.asm, does the LED blink using GHS IDE and compiler?
.bss
.org 0x08000000+0x00001000+0x00000100
__ghsend_stack::
Hi Spoorthi,
Spoorthi M said: 1) Check the above reference and please provide the code for data communication between HDK board and e xternal hardware (data key) .
The provided code can also be useful to get data from external hardware,
did you try by disabling…
Part Number: TMDX570LC43HDK Are there any example code on how to read/write data to the SD card on this board, with or without a file system? (Obviously a file system will be better)
Part Number: TMDX570LC43HDK Hi everyone,
I'm trying to get started with a sample project in Code Composer Studio, using the eval board TMDX570LC43HDK. Unfortunately, I can't seem to get very far using the Project Wizard (Project -> Project Wizard (Resource…
Trivedi said: Does the eval board require two connections to make it work?
Yes. USB cable is used for XDS100V2 emulator and virtual COM port (SCI1).
Trivedi said: There is only one blue LED powered on while I plug the USB cable.
Please plug in the power…
Part Number: TMDX570LC43HDK Hi Team,
In the month of May 2022, we purchased TMDX570LC43HDK and executed an example experiment "UART communication 9600" whose output is seen on tera term. After that, when we tried to load the program, an error…
Part Number: TMDX570LC43HDK Other Parts Discussed in Thread: LAUNCHXL2-570LC43 Good morning,
is it possible to have a detailed description about the differences between the development boards TMDX570LC43HDK and LAUNCHXL2-570LC43.
Thanks
Part Number: TMDX570LC43HDK After the new project is built, the RED error indicator is always on.I checked the connection below:but the supplied CMD file cannot be opened.The program cannot run after modifying flash settings.
Console always shows:CortexR5…