Oops, I'm so sorry. I forgot about this post.
This problem is solved. The cause was a version issue. I made and tested a host for ICSS_PRU and it works well. I so appresiate Dhaval.
Best regards hakjun, oh
Part Number: TMDXIDK5718 hi.
I am currently reviewing the functionality of the board and have identified the need for the operation of a multicast server in order to configure DLR. However, I have noticed that the NDK has the define of IP_ADD_MEMBERSHIP…
Part Number: TMDXIDK5718 HI,
I am working on the TMDXIDK5718 board with processor sdk version 06_03_00_106
As per requirement of my project I need to boot the uboot using uart or code composer studio but according to the processor sdk version 06_03_00_106…
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: TPIC2810
Hi,
I am trying to write to the locations in ddr3 it is showing like this.
root@am57xx-evm:/usr/include/linux# devmem2 0x4843E20A w 0x00000001 /dev/mem opened.[ 677.863057] ----------…
Ryan Sorry for the delayed response here.
Ryan Hodgman said: Wanted to check if there was any update on the Sync1 Start Time Register issue at startup?
In this case, can you check when does the master update SYNC1 Cycle Time (0x09A4-0x09A7) register? Is…
Hi Mounika,
Parth Nagpal said: Also, there are some standard test cases available at /opt/ltp that you can try.
As I mentioned there are some test cases available at the path above, but apart from that you'll have to write your own test cases. Regards…
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: AM5718 Hi,
I am using am5718 idk and my SDK version is 6.03.00.106 Linux. I want use a pin to gpio then how can I change the dts file related to that. Explain with an example.
Regards,
Bhardwaj…
Part Number: TMDXIDK5718 Hi,
I'm using SDK-LINUX-AM57X 06_03_00_106 on TMDXIDK5718.
I want to connect to 10BaseT hub by using Eth2.
Eth0 and Eth1 work well, but Eth2 - 5 don't work.
"ethtool" shows Eth2 - 5 are not supported.
Please…
Part Number: TMDXIDK5718
Hi, I am working on TMDXIDK5718 board
Can I get the procedure to flash the board through sdcard or through Code Composer Studio IDE