TMP1075 can be configured for 32 different I2C addresses.
TMP144 has a UART interface that can daisy-chain 16 devices. TMP107 has a similar UART interface that can daisy chain 32 devices, but the SOIC package would probably not appeal to you.
thanks, …
Part Number: SN74LVC07A Other Parts Discussed in Thread: TMP144 , , TXU0204
Hello,
I am working on an application where I plan to interface a TMP144 temperature sensor (which operates at 3.3V logic levels & 5kbps baud rate) with a 5V UART logic field…
Hello Clemens,
When using SN74HCS125 - can we use multi channles in parallel to increase the effective capacitive drive strength?
We have to interface TMP144 sensors to our MCU UART & we are planning to use the SN74HCS125 (already in inventory) for improved…
Yes, it is standard UART. It is being generated at the PC and only passes through the MSP430F5528. In the TMP144EVM GUI, this happens in the file UARTPacketCodec.js which is located here: https://dev.ti.com/gallery/view/THSApps/TMP144EVM/ver/1.0.1/app/UARTPacketCodec…
Hi,
The waveform I send was a working example waveform on a similar device, the TMP144, which has the same protocol. Attached is full transaction with the TMP144.
Your Stop bit also seems to be four time as long as the braud after the calibration byte…
Hi Shotaro-san,
The TMP103 accuracy over temperature is shown in Figure 10.
Since the resolution is only 1C, it may not be practical to improve the result with calibration.
What is your accuracy requirement? Have you considered TMP108, or TMP144?
thanks…
Part Number: TMP103 Other Parts Discussed in Thread: TCA9548A , TMP1075 , TMP144 , TMP104 Hi,
What's the input capacitance for the I2C pins on the TMP103? Any concerns with attaching 6+ TMP103 onto the same bus?
Thanks,
Peter
Part Number: TMP116 Other Parts Discussed in Thread: LMT01 , LMT87 , TMP468 , LMT70 , TMP108 , TMP468EVM , TMP144 , TMP411 Hello everyone,
In one of my design, I need to sense MOSFET temperature or/and inductor temperature (TDSON package) which is NOT at ground…
Part Number: LAUNCHXL2-RM57L Other Parts Discussed in Thread: RM57L843 , HALCOGEN
Tool/software: TI C/C++ Compiler
The attached project was created in CCS 10, targeting a RM57L843 using source code generated by HalCoGen. The project selects the GNU v7.2…