Part Number: TMS320C6203B Tool/software: Hi,
I know that the C6203B is a very old processor but I think this issue could be reproduced in newest versions. I do not want to focus it on the DSP version, so any approach will be apreciated.
Is Is…
Part Number: TMS320C6203B Tool/software: hello
I have a library compiled as .lib that I want to add in the SDRAM section of my main project that will run in FLASH. I want to add it in such a way that the .text section of the library goes to a SDRAM_CODE…
Part Number: TMS320C6203B Good afternoon
Please, could you indicate me what is the Maximum Junction Temperature (ºC) for the component TMS320C6203BGNZA250 ?
Thank you in advance
Marisa de Diego
Part Number: TMS320C6203B In context, the development environment we want to use is Code Composer, in one of its versions from 2.21 to 5.5. These versions are compatible with a Windows 10 32-bit framework and they can be installed in Windows 10 Pro 64…
Part Number: TMS320C6203B Dear Mr. /Mrs.
I would like to know the Juntion Temperature of the TMS320C6203B DSP. In the datasheet is only available the operating case temperature:
Thanks in advance,
Best regards.
Carlos Antón.
Part Number: TMS320C6203B Hello Team,
My customer have relaunched an old project in which software development was based on Texas development environments, and both Code Composer 2.21 and the XDS510PP JTAG probe were used.
We have seen that this…
Part Number: TMS320C6203B I am trying to look for information on this topic, but the only thing I have found in particular is in the spru642.pdf the 3 boot-modes: No boot process, ROM boot process and Host boot process. It seems that none of these three…
Part Number: TMS320C6203B Is there any data or analysis TI can provide for meeting DO-254 for this processor, or in declairing this device as "Simple" or "Complex" hardware for DO-254 application.
Michael,
C6203B is pretty old. I would suggest using CCSv3.3 which is available on the CCS download page:
http://software-dl.ti.com/ccs/esd/documents/ccs_downloads.html#code-composer-studio-version-3-downloads
Note that CCSv3.3 itself is very…