Part Number: TMS320C6416T Hello,
Could you please recommend a military grade product that has the same or similar features as the TMS320C6416TBGLZA6?
Thank you.
Part Number: TMS320C6416T To whom it may concern
We would like to change the material TMS320C6416TB G LZA6 to TMS320C6416TB C LZA6
When I checked the datasheet, the difference between G and C is confirmed as ROHS difference.
I would appreciate it if you…
Part Number: TMS320C6416T Hi TI experts,
I need to write a simple program for TMS320c6416t to blink an LED on a gpio pin, for this I use CSL.
Immediately I got a problem when calling the CSL_init function, I get the following errors
the CSL_init function…
Part Number: TMS320C6416T Hello all,
I have dev board with TMS320C6416t, emulator XDS100 v3, jtag connection test is fine, but when I run the debugger I get the error:
Error connecting to the target: (Error -1004 @ 0x0) Device is not responding to the…
Part Number: TMS320C6416T Hello,
I have a question regarding optimization problem.
Here is my code:
/*Loop for correlation computation.*/
for (n1=0; n1<1400; n1++) { fine_sync = 0.0+0.0*I; for (m1=0; m1<200; m1++) { fine_sync += mpysp(input…
Part Number: TMS320C6416T Hello,
If we have purchased a large quantity of TI products (evaluation models), can we purchase training/support for that? I understand that TI doesn't provide support for C6416T DSP, but can we purchase support for that?…
Part Number: TMS320C6416T Hello,
With reference to the question about software reset to dsp, CCS version 6.1.3, EVM: Dsk6416.
I want to reset dsp from my code running in dsp.
Means, when I start debugging session, I want to give reset to dsp using my…
Part Number: TMS320C6416T Hello,
I am using TMS320C6416T. I am using EDMA controller to transmit two different message formats. Firstly, I am transmitting a message format of 9 bytes and then extending the buffer size to 30 bytes. When I reconfigure the…
Part Number: TMS320C6416T Hello,
I am using DSP/BIOS v5.42 on CCS v6.1.3 with TMS320C6416T dsp. Since installing DSP/BIOS, whenever I run a project containing std.h source file, I get an error that could not open source file std.h although I have included…
Part Number: TMS320C6416T Hello, I am configuring EDMA interrupt using DSP/BIOS v5.42 on CCS v6.1.3 and I am using DSK6416T DSP. I have designated ISR for HWI_INT8 from the properties as _edmaHwi where edmaHwi() is the name of my C function. I am also…