Titus,
We are making progress :-)
Using the 2th method, I got 9 clock cycles out of the I2C SCL (see code below) :-)
Two issues that need further investigation:
1) the SCL bus was stuck low after the 9 clock cycles! I had to issue a reset command…
Dear Team,
Could anybody kindly tell me where can I download the materials in the kit disk?
I have bought one EVM but my disk lost and I didn't backup all the contents.
Thanks in advance for your kind help.
B.R.
Other Parts Discussed in Thread: BIOSLINUXMCSDK Hi Raja,
Could you help to share the whole "McBSP as I2S " project with me ?
Or could you please help to complete the project? I have already copied the codes in the application note. The head files…
Hi All,
I have trouble finding information what value the srcTID/targetTID fields will be set for SRIO packets sent by the DSP. I have checked the following documents so far: "TMS320C6472/TMS320TCI648x DSP Serial RapidIO (SRIO) User's Guide" and "TMS320C6472…
Luca,
Wishes for your experiment with NDK. The CSL have the EMAC module API, already you mentioned using the biossdk. you see the CSL code at : http://www.ti.com/tool/sprca03 Go through the TMS320C6472 Chip Support Library API Reference Guide get more…
Hi,
I run the helloworld from the mcsdk on the smt372t with carried board smt111. The console print message as follows:
TCP/IP Stack "Hello World!" Application
Registration of the EMAC Successful, waiting for link up ....
Network Added: If-1:192…
Hello,
I'm using the TMS320C6472 DSP(8 cores).
The first three letters on the second line of the printing on the chip is "N21" which means that the silicon revision of the chip is 2.1.
When i read the ID register of the device using JTAG i see that…
hello,
I tried to run a project on TMS320C6472-EVM board with XDS100USB emumlator using CCSv4 but I found many problems.
Please I want know the details to run a project on this board(target configuration, DSP/BIOS configuration...)
Can you send…