Other Parts Discussed in Thread: OMAP-L137 , TMS320C6743 , CC2538 , OMAPL138 Hi, I'm trying to design a system using a TMS320C6743 to perform some signal equalisation. The DSP will be as an SPI slave to a CC2538 master microprocessor. I've got the OMAP-L137…
Ray,
Since the SM320C31 is a DSP processor, I would recommended the C674x family of devices.
These include the:
TMS320C6742
TMS320C6743
TMS320C6745
TMS320C6746
TMS320C6747
TMS320C6748
Regards,
Kyle
Hannah,
The current DSP devices that we are actively providing support on are the C674x family of DSPs.
This includes the following:
TMS320C6742
TMS320C6743
TMS320C6745
TMS320C6746
TMS320C6747
TMS320C6748d
Regards, Kyle
Other Parts Discussed in Thread: TMS320C6743 , TLV320AIC23B Sir,
I have to interface audio codec TLV320AIC23B with TMS320c6743 DSP. In the codec specifications
it is mentioned that it can be Software Controlled Via TI McBSP-Compatible Multiprotocol Serial…
Other Parts Discussed in Thread: TMS320C6743 Hello,
Part: TMS320C6743
1) I want to confirm that the TMS320C6743 can (albeit
inefficiently) execute code from Flash. My customer suspects that their software may exceed the size of the internal memory …
Hi Nate,
Thanks for the advice! I followed your instructions, and it doesn't seem to be an SDK or package problem. When I rebuild, I still get the following console output:
**** Clean-only build of configuration Debug for project odsdemo_16xx_dss…
Hi, Colin,
In the C55x FAQ, TI suggests:
You may also want to consider evaluating a C6000 fix and floating point DSPs as a migration path. While they are not direct replacements for the various C5000 DSPs.
TMS320C6742: http://www.ti.com/product/TMS32…
Part Number: AM5726 Other Parts Discussed in Thread: SYSBIOS Hi,
I'm working with a project I created based off of the GPIO_LedBlink_evmAM572x_c66xTestProject example from the evmAM572x processor SDK. I followed the instructions in the PSDK Linux developer…
Part Number: TMS320C5535 Another post in the E2E forum said that the C5000 devices are NRND, so the TMS320C5535eZdsp shouldn't be used.
Could you please recommend a compatible board that's also affordable for students to buy?
The FAQ listed on…