Part Number: TMS320DM368 Hi.
Hi I'm trying to configure the H.264 encoder and change rate control mode.
So I Changed Ratecontrolpreset and results out followings;
1. IVDIEO_NONE => Compile Success , Executable file Success
2. IVIDEO_LOW_DELAY =…
Part Number: TMS320DM368 Hi All
I ran the H.264 codec using DM368EVM, but the 1080p processing time is 37ms / frame.(About 27fps) Please tell me what kind of parameter setting is required to operate at 30fps.
<--- Encode Params ----------------------…
Part Number: TMS320DM368 hi,all.
My customer uses a DM368 custom board.
Outputs 1080p30 digital video in external sync mode. I tried changing the register settings such as HSTART/VSTART, HSDLY/VSDLY, and OSD_BASEPX/Y, but I cannot output the image of 8…
Part Number: TMS320DM368 Tool/software: TI C/C++ Compiler Hi Sir,
The TMS320DM368 uboot Just started to use the boot is no problem, to the client for a period of time there is a probability that the system can't be successfully started u-boot, the…
Part Number: TMS320DM368 Tool/software: Code Composer Studio hello I have question I use dm368 and video source is ir camera(ntsc) Blurring occurs in the bottom third of the image below.(red box) I am wondering if the following problem occurred in TI enc…
Part Number: TMS320DM368 Hi Team,
We are currently using TMS320DM368ZCE48 for a design and there is no more stock. Would TMS320DM368ZCEF or TMS320DM368ZCED48F work as a drop in replacement?
Regards,
Garret
Part Number: TMS320DM368
Part Number: TMS320DM368 Hi, What's the difference between TMS320DM368ZCED and TMS320DM368ZCEDUP ? Can customer use TMS320DM368ZCED to replace TMS320DM368ZCEDUP ?
Part Number: TMS320DM368 Hi Team, Our customer needs some clarifications concerning the suffix "48" on TMS320DM368ZCE48. The post below says that it represents its clock speed, which is 468MHz. Is this the only difference of the device from TMS320DM368ZCE…
Part Number: TMS320DM368 Hello,
Our system scenario is SVGA input -> ADV7181C decoder -> DM368 -> TV out/ Streaming over ethernet.
Configuration parameter are:
16 bit data with externel Vsync and Hsync
frame rate 60
YUV 422
HD polarity = P…
Part Number: TMS320DM368 Hi, I have a question from my customer for JTAG pin handling. If JTAG pins are not in-use, what are recommended connection on board(PU, PD, NC) for each pin? TCK : PU? TDI : PU? TDO : NC? TMS : PU? nTRST : PD? RTCK : NC? EMU0…