Part Number: TMS320DM648 Hello team,
Customer is having a reliability problem with the 2 nd 1G port on the DM648 after boot.
Do we have any errata documents on the 1G ports for the DM648?
Do we have a newer version on the boot loader code for customer…
Part Number: TMS320DM648 in doc spruem2a, Dm648 supports only 16-bit adress,because it uses a 16-bit-long register for memory adress;
in the meanwhile, in the erf spraaj1d, 24-bit SPI address mode is valid.
I wonder that dm648 is able to boot from spi…
Part Number: TMS320DM648 Hi,
Would you pls kindly advise what's the "HK" means in TMS320DM648ZUT9HK?
My customer wants to know the difference between TMS320DM648ZUT9HK and TMS320DM648ZUT9. I can't find info about "HK" in DM648 datasheet…
Part Number: TMS320DM648 Hey,
My system uses DM648. We are connecting to other system, using ethernet port.
Right now we are unable to connect (no link) to the other system directly, only via switch. I am suspecting the problem is the 2 systems are set…
Part Number: TMS320DM648 Hello,
I saw a strange phenomenon of DM648 timer interrupt. DM648 has up to eight 32-bit timers. I've used five timers, I'll add one timer for updating software. Since I need six 32-bit timers, I can avoid using TIM34 of Timer…
Part Number: TMS320DM648 Hi,
we use llpacket API. In order to implement an own protocol we parse the ethernet frame in llPacketService. Works so far except that the ethernet header of frames with VLAN tag are not correct when we receive it on the Dm648…
Part Number: TMS320DM648 Hi, i was looking for an 64/128 Mb emif memory chip for this DSP, but i dont see any memory on ti, and i dont see any company that have memory and tag it with emif connection, so im not sure what chip i should choose.
So long…