Other Parts Discussed in Thread: TMS320F28044 , CONTROLSUITE Hi, I need some help regarding IFFT and FFt Is there any library supplied by TI that contains IFFT (Inverse Fast Fourier Transform) functionality that can be used with the TMS320F28044 (Fixed point…
Other Parts Discussed in Thread: TMS320F28044 Hi, I need some help regarding IFFT and FFt Is there any library supplied by TI that contains IFFT (Inverse Fast Fourier Transform) functionality that can be used with the TMS320F28044 (Fixed point)? I am using…
Other Parts Discussed in Thread: TMS320F28044 I have a TMS320F28044 eZdsp board and am running CCSv4 on Windows Vista. I'm trying to load a program onto my board, but the Connect Target button under the Target drop down menu is grayed out so that I cannot…
Other Parts Discussed in Thread: TMS320F28044 hi all
i want to copy code into on chip RAM from Program memory,
i am using TMS320F28044 device, and unable to know exact wait state require for Flash.
please see this post (http://e2e.ti.com/support/microcontrollers…
Other Parts Discussed in Thread: TMS320F28044 Hi.
I use the TMS320F28044 to generate the PWMs for a six phase DC DC converter with High Resolution. Currently the ePWM1 is the master and generate the SYNCO at CTR=ZERO. The other ePWMx are synchronized…
Other Parts Discussed in Thread: TMS320F28044 I am doing an ultrasound design using a TMS320F28044. My need is to generate a chirp waveform, and then after a suitable delay start sampling the received waveform using the ADC.
In connection with this, I…
Other Parts Discussed in Thread: TMS320F28044 , LM317 hi all,
i have design a system using TMS320F28044 processor and
power supply using LM317.
i am using two 317 ic's for 3.3v and 1.8v,
first ic regulate 3.3v from 5v while second ic regulate 1…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
Chris,
Along with the help of tech support and the resources you provided, I've made some progress with the peripheral explorer kit. I am able to utilize all functions with the GUI. However, now I am needing to start using the TMS320F28044 controlCARD…