Other Parts Discussed in Thread: TMS320VC5505 hai
i am using the tms320vc5505 usbstick by using the timers in the module is it possible to generate the software pwm outputs to gpio pins to drive some loads.
with regards
seeni
Other Parts Discussed in Thread: TMS320VC5505 hai
i am using the tms320vc5505 usbstick and by enabling the timer and i toggle the led for every 50ms it works fine when we run in the initial stage and after some time it automatically stops the timer and…
Hi Kumar-san,
Thank you for your information.
I understand that this is not EOL.
Why doesn't the VC5504 product page exist? Can I get a datasheet for this device?
Best regards, Sasaki
Sasaki-san:
This is the best information I can point you to:
Silicon…
Other Parts Discussed in Thread: TMS320VC5505 , SPRC133 Hi,
I want to use the DSP BIOS with the TMS320VC5505 and the AIC3204. I found a simular example that uses the C5510. I want to port that code to 5505 board, and i can not resolve the CONTROLLER_FXN_TABLE…
Other Parts Discussed in Thread: TMS320VC5505 hi
i have a TMS320vc5505 EVM and i need to use SAR ADC to convert an analog signal. I wrote below assembly code but it didn't work:
;********************************************************************…
Other Parts Discussed in Thread: TMS320VC5505 Hi all,
I am working on a project with the dsp device TMS320VC5505 . I would like to connect multiple LEDs to a GPIO, but in the data sheet does not show the maximum current in this type of ports. I 've loo…
hi there,
i need your help , i have a TSM320VC5505 eZdsp USB stick and i run the example aic3204, i gave some sounds the input so data1 and data2 equals zero and data2,data3 equlas around -108, i didnt give a sound input and result is the same why?
what…
Hi,
Apologies for the newbie question but I have been searching the Chip Select Library for vc5505 DSP in order to find out how to put it in sleep mode but the documentation (generated by doxygen) contains no documentation on how to enable sleep mode…
Other Parts Discussed in Thread: TMS320VC5505 hai
i am using the tms320vc5505 ezdsp usbstick in this kit i added the spi shift register when i run the test program for the spi_rom i see the activity on the bus but when i try to run the chip support…