Part Number: TMS470R1B1M Other Parts Discussed in Thread: SM470R1B1M-HT i have two confused questions about TMS470.
First, i can't config 6 PWM by using HET. The code is list below. And there are only two PWM out(pin1 and pin2). How can i config HET to…
Part Number: TMS470R1B1M Other Parts Discussed in Thread: SM470R1B1M-HT , I am using DMA transfer in conjunction with SCI3 receive function. Everything seems to be working with one exception: When I receive less than the number of characters specified in…
Part Number: TMS470R1B1M I'm using one of the older TMS470 parts (TMS470R1B1M). I have configured the SPI1 and SPI2 lines as GIO and am using them as inputs. When the pins are not connected to anything, they appear to be floating. Is the no internal pullup…
Part Number: TMS470R1B1M when debug,code running correctly,but download hex into flash,then reset MCU,it dont run,who has some suggestion for me,should i change .icf file?
tks
best regards
Part Number: TMS470R1B1M Other Parts Discussed in Thread: SM470R1B1M-HT HI:
where can i find function"Flash_Prog_B",when i called this function,compiler told me "no definition for Flash_Prog_B ",is it included in a library? thks,i use source Insight to…
Part Number: TMS470R1B1M Hi all,
I'm having issues programming a TMS470R1B1M
I have four identical boards each withthe same microcontroller and batch code CA-41C91W. One programmes without a problem the other 3 fail with the same error "CPU-failed…
Hi,
This is an EOL'ed device. Its architecture is similar to https://www.ti.com/product/TMS470R1B1M for which you can find the TRM. There is no HalCoGen for this device.
Part Number: TMS470R1B1M Other Parts Discussed in Thread: SM470R1B1M-HT Hi,
Please suggest alternate part for IAR J-Link compatible with TMS470R1B1M and IAR Workbench
Other Parts Discussed in Thread: TMS470R1B1M , HALCOGEN , LAUNCHXL2-RM46 , LAUNCHXL-RM42 Hi,
Do you know any smaple code on how to use tap interrupt on TMS470R1B1M?
Thanks, Jian