Prasad,
I apologize as this was missed as well when it was moved to HiRel Forum.
Unfortunately there is minimal collateral available.
Have you referenced the Software Peripheral Drivers (SPD) in the product folder? There may be some code help there.
…
Hello Jian,
Given the length of time that this thread has remained open without any activity, I assume your question has been answered and it will be closed. If possible, please take the time to verify the post that provided the most useful answer in…
Other Parts Discussed in Thread: TMS470R1B1M , SM470R1B1M-HT Hi,
I am using IAR system IDE from ARM to develop firmware for TMS470R1B1M, the output file extension can be .out, .srec, .sim, or .hex, .bin.
Is there a flash programmer to download this file…
Other Parts Discussed in Thread: TMS470R1B1M Hi,
I need to develop bootloader for the TMS470R1B1M device. Is there any sample code I can get started?
Thanks, Jian
Hi Folks,
I am a newbie in this bootloader development. i need to develop a bootloader for SM470R1B1M(ARM7TDMI core) device in which i have to read the application firmware from the external flash via SPI, and update it onto controllers internal flash…
Other Parts Discussed in Thread: TMS470R1B1M , SM470R1B1M-HT Hi,
I know TMS470R1B1M is old. Do you have replacement part? We are using it for drilling downhole application, has to be high temperature rated.
Thanks, Jian
Hi Folks,
I am a newbie in this bootloader development. i need to develop a bootloader for SM470R1B1M(ARM7TDMI core) device in which i have to read the application firmware from the external flash via SPI, and update it onto controllers internal flash…
Other Parts Discussed in Thread: SEGGER , TMS470R1B1M Hello, I have problem to record a TMS470R1B1M flash, flash lei perfectly, I wanted to rewrite it to make a test, but I pulled the error message (blocked field), I am haceindo with Segger J-link, I hope…
Other Parts Discussed in Thread: TMS470R1B1M Hi,
I am using TMS470R1B1M. I have enabled ADIN[0] to ADIN[4], meaning I use the first 5 internal AD channels of group 1. And interrupt is enabled.
The problem is if I enable all 5 channels, the ADC0, ADC1,…