Hello Patrick
I'm not sure about internal structure of shutdown, but your circuit could be similar to the real circuit.
You could have a look to the TPA4861 is a Class AB amplifier. Other options are TPA2001D1 or TPA2005D1 are Class D amplifiers…
We've been noticing a lot of requests for similar parts to replace the NXP devices that are being discontinued. I've made a comprehensive list for these NXP devices and their TI replacements below. Note: they are not pin-to-pin replacements; they are…
Hi, Kevin,
1. You're right. LINE1LP, LINE1RP, LINE2LP, LINE2RP, MIC3L, MIC3R are used as single-ended.
2.
For 1W amplifiers, I would suggest to take a look at the following devices: TPA2005D1, TPA2001D1 and LM4890.
For 3W amplifiers, I would…
Other Parts Discussed in Thread: TPA2005D1 , TPA2001D1 Hi Team,
I' d like to ask about short-circuit protection of TPA2005D1.
Is short-circuit protection of TPA2005D1 the same as TPA2001D1?
It seems TPA2001D1 has the protection under short to Battery…
Hi Toshi
The TPA2001D1 meets the requirements. You could use the TPA2005D1 or TPA2006D1 too. But they have an output power a little bit higher than 1W. I recommend you to take a look these devices.
Please let me know if you have more questions.
Best re…
reda38 said:
My question is : is the DaVinci DM365 powerful enough to power a loud speaker of let's say between 0.5W to 1W power ?
Based on the TMS320DM365 datasheet in Section 6.26, the integrated voice codec is able to drive a 200mW to 300mW speaker…
Other Parts Discussed in Thread: TPA711 , TAS5630 , TAS5615 , TAS5613 Class AB amplifier efficiency in SE configuration
Q: Class AB amplifier efficiency in SE configuration
A customer wants to use a TPA711 in SE mode to drive a 15 Ohm speaker. Could you provide…