Part Number: TPD1E05U06-Q1 Hello Team,
My customer wants to know how much capacitance value when Vio set to 0V.
The datasheet mentions DPY package IC has 0.42pF at Vio set to 2.5V.
However, no data at Vio set to 0V.
could you please provide capacitance…
Part Number: TPD1E05U06 Other Parts Discussed in Thread: ESD401 , TPD2E009 Hey team,
Hope everyone's having a great day. I need a drop-in for PESD5V0X2UAM ( webpage & datasheet ), which I doubt is available but if I could at least get some recommendations…
Part Number: TPD1E05U06-Q1 Dear team,
My customer uses this device for USB 2.0 interface. H3 and H4 are two USB pins. The CAR OEM has a requirement that they need to test LCR of USB signal pin before and after ESD test(power down mode), and then make …
Part Number: TPD1E05U06 Other Parts Discussed in Thread: TVS0500
I see some words in datasheet from other vendor, such as GESDPSA0402V05 (steifpower.com) , it states:
Caution: This component is designed for signal line protection only, Not intended to…
Part Number: TPD1E05U06 Hello team,
Could you please let me know how to protect LED from ESD?
In my system, +5.7V rail is connected to diode anode. The kathode is connected to drain of optoMOS.
Please find the internal link here for partial schematic…
Part Number: TPD1E05U06 Other Parts Discussed in Thread: STRIKE Hello,
I'd like to ask what is the purpose of the diode in red circle on the picture attached?
Wouldn't the circuit work without this diode the same?
Probably the answer is simple…
Part Number: TPD1E05U06 Hi
Why is TPD1E05U06 employed the structure of left side instead of right ?
Please kindly advise the benefit.
Thank you and best regards,
Michiaki
Part Number: TPD1E05U06
Hi Team,
The figure 5 shows the leakage current under different temperature, may I know if there is similar curve when the Vio is 5V and -0.2V?
The datasheet doesn't have capacitance vs frequency curve, the picture below is taken…