Part Number: TPD1E05U06-Q1 I am using the TI TPD1E05U06-Q1 TVS to protect my USB 2.0 DP & DN lines that are connected to a FTDI FT601 chip and the the communication is failing. I measured approx 800mV on the DP and close to 0V on the DN lines. When I removed…
Part Number: TPD1E10B06 Other Parts Discussed in Thread: TSD05C , , TPD1E05U06-Q1 , ESD1LIN24 , Hi, I am looking for ESD protection for my 5v MCU inputs and outputs. Is this the ideal component for this application? Just put this next to the connector with…
Part Number: TPD1E05U06-Q1 Hello,
It looks like polarity marking for TPD1E05U06-Q1 is wrong.
Pin 2 should be marked as cathode.
can you please confirm this as soon as possible ?
Thanks and Regards
Vijay
Part Number: TPD1E05U06-Q1 Other Parts Discussed in Thread: TPD1E05U06 Dear Support team
Could you provide recommended pattern layout for protection of LVDS differential line?
I want to know the position of the IN+ and IN- of deserializer and coupling…
Part Number: TPD1E05U06-Q1 I have a design using the TPD1E05U06-Q1 to protect our USB 3.0 Type C signals. We have just completed the initial routing for these signals. Is there someone from TI who can look at the routing and check it ?
Part Number: TPD1E05U06-Q1 Other Parts Discussed in Thread: TPD2E2U06-Q1 Dear support team;
I downloaded s-parameter model from the following site.
- TPD1E05U06-Q1
www.ti.com/.../slvmbu0
- TPD2E2U06-Q1
/cfs-file/__key/communityserver-discussions-components…
Part Number: TPD1E05U06-Q1 Hello,
We are having a problem with the TPD1E05U06-Q1. The device is on a line that has 1.6V and is in breakdown holding the line at 900mV. we did not expect breakdown until 6.5V via the datasheet. Do you know what could cause…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Part Number: TPD1E05U06-Q1 Other Parts Discussed in Thread: TPD4E05U06-Q1 , ESD122 , TPD1E05U06 I am using these diode with our USB 3.0\USB 3.1 IOs, however we are having trouble with the routing. Are there any other smaller components available (it would…