Other Parts Discussed in Thread: TPD1E10B09 , TINA-TI , THVD1450 Hi all,
I was looking for TINA-TI model for TPD1E10B09 and THVD1450, and found IBIS models only.
Are there TINA-TI models available for TPD1E10B09 and THVD1450?
Regards,
Kutumi Hasegawa
Part Number: TPD1E10B09 Dear Ti and all,
For ESD issue, I apply ESD suppress(TPD1E10B09, and ETC).
But the audio signal is too low than before applying that part.
Below, I attached a circuit file.
Please, review my circuits.
Audio_Devices.pdf
Thank you…
Part Number: TPD1E10B09 Dear all, could you please help provide the Safety report of TPD1E10B09? The EMC test house requests this report. Because TPD1E10B09 is a ESD protect component. It needs a report to prove(such as UL、VDE or TUV). Thanks.
Hi Gideon,
Here is a good reference thread about ESD protection for 3.3V CAN, I agree that ESD2CAN-Q1 is not the ideal option for TCAN334 on transient surge protection.
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1066366/tcan332g…
Part Number: TPD1E10B09 Datasheet of TPD1E10B09 is described "Place pin 1 on the signal line" on page 8 and page 10.
When connect reverse polarity (pin 2 on the signal line), what is occur problem?
I think that TPS1E10B09 have no polarity and…
Part Number: TPD1E10B09-Q1 Hi Team,
I am considering using the TDP1E10B09-Q1 in an automotive application where it is protecting lines that go off board. This means those lines are susceptible to a short to battery condition up to 18V. I noticed the breakdown…
Hi,
For automotive, we don't have an automotive version of ESDS552 which is 12V in our portfolio currently. But for 24V, there are more options. There is ESD1LIN24-Q1 , ESD751-Q1 , and ESD761-Q1 which are all SOD323 or smaller and the main difference…
Part Number: TPD1E10B09 Other Parts Discussed in Thread: ADS1292 , STRIKE , ESD401 , TPD1E10B06 Hi,
I'm using the TPD1E10B09 (Single-Channel ESD Protection Device in 0402 Package). The datasheet states IEC 61000-4-2 to +/-20KV Contact Discharge.
In our…
Part Number: TPD1E10B09 Other Parts Discussed in Thread: STRIKE , MSP430FR2433
Hi,
I am planning to use TVS diode TPD1E10B09 for ESD surge protection. The general convention is outer edge of the microUSB is connected to the ground, so any ESD strike happens…