Part Number: TPD2E1B06 Hello,
I wonder what the leakage current is for the specified VRWM Reverse standoff voltage of 5.5 V (regarding the component TPD2E1B06).
In the datasheet the leakage current is only given for a VBIAS = 2.5V (max 10nA).
In other…
Part Number: TPD2E1B06 Dear Sir,
MY customer complained the CL2 value will cause their system function fail!
In datasheet, the typ. value of CL2 is 1.05pF, but it is not a fixed value and did not provide the min. and max. range!
My customer found IC…
Hi Gideon,
Here is a good reference thread about ESD protection for 3.3V CAN, I agree that ESD2CAN-Q1 is not the ideal option for TCAN334 on transient surge protection.
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1066366/tcan332g…
Part Number: TPD2E007 Other Parts Discussed in Thread: TPD2E1B06 Hello,
I have a question about the difference between schematic of TPD2E007 and TPD2E1B06.
[Q] - Schematic of TPD2E007(D/S p6)
- Schematic of TPD2E1B06(D/S p1)
What are the intentions of…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation and Temperature
Top…
Apologies for the 2 days late reply,
Here is the schematic. I think i did it correctly, on me though for not noticing it in the posted post
I based this circuit on the example circuit given by the datasheet, the TPD2E1B06 is just an ESD protection…
Other Parts Discussed in Thread: ESD122 , ESDS302 , TPD2E1B06 , TPD2E007 Hi,
I am looking for replacements that has a package larger than ESD122DMXR and TPD2E007DCKR.
These parts are too small to mass-produce.
ESD122DMXR is used for USB and LVDS.
TPD2E007DCKR…
Part Number: ADS1147 Other Parts Discussed in Thread: TPD2E1B06 Tool/software: Linux Hi,
Right now I try to evaluate the ADS1147, but I cannot find a application for ESD, Burst or Surge.
I am specially interessted in the 3 Wire Ratiometric RTD Measurement…
Murat,
Looking at the allowable voltage ranges for the different protocols:
SPECIFICATIONS
RS232
RS423
RS422
RS485
Mode of Operation
SINGLE
SINGLE
DIFFERENTIAL
DIFFERENTIAL
-ENDED
-ENDED
Maximum Driver Output Voltage
+/-25V
+/-6V
-0.25V…
Hi Karl,
I was out of office yesterday, you should get a message today.
So the series resistor in the TPD2E001 datasheet appears to be a throwback to USB 1.1 where series resistors in DP/DM path were much more common, it is not a required value. Also…