Part Number: TPD8S300 Other Parts Discussed in Thread: TUSB564 , TPS65982 , Hi Team,
My customer uses the TPD8S300, TPS65982 and TUSB564 in an UFP application.
We noticed that the abs max. rating of the SBU pins of the TUSB564 is 4 V while the min. SBU OVP…
Part Number: TPD8S300 Other Parts Discussed in Thread: TPS65981EVM Hi,
For a USB type-C UFP design, Where do we need to have RPD_Gx pins shorted to CCx pins for dead battery condition?
1. Is it near TPD8S300 side only?
2. Is it near TPS65986 side only…
Part Number: TPD8S300 Other Parts Discussed in Thread: TPS65983B Hi Team, Could you please help review the TPD8S300 schematic and layout? the password is "ti". U7605 TPD8S300 U7613 TPD8S300
TBT_TPS65983B_dualport.7z
Thanks, SHH
Part Number: TPD8S300 Other Parts Discussed in Thread: TPS65981 , TPS65981EVM , , TPD4E05U06 Hello,
I’m looking for ESD devices for USB Type C I/F which uses TPS65981.
The TPS65981EVM uses TPD8S300.
But in my case, only CCx and D+/D- signals are used…
Part Number: TPD8S300 team, may I know the TI spec for this item?
Thanks.
Grp
Component Description
Component Spec
P/N
V spec.
I (mA) spec.
Tspec. ( ℃ ) Ta
Tj Spec.
Pd (mW)
R θj-c ( ℃ /W)
…
Part Number: TPD8S300
team, may I know the TI spec for this item?
Thanks.
Grp
Component Description
Component Spec
P/N
V spec.
I (mA) spec.
Tspec. ( ℃ ) Ta
Tj Spec.
Pd (mW)
R θj-c ( ℃ /W)
…
Other Parts Discussed in Thread: TPD8S300 , TPD2S300 , TPD2S703-Q1 Hi Team
I see there is TPD8S300, but it protect CC/SBU/DP-DM. Do we have have individual DP/DM short to Vbus OVP protector? For example, there is TPD2S300 which protect CC individually. Thanks…
Part Number: TPD8S300 Dear Team,
What's the CC1,CC2 and C_CC1,C_CC2 voltage when floating?
My customer feedback that their measurement result is CC1/CC2 are 0.35V and C_CC1/C_CC2 are 0.6V.
Is this normal?
BTW, the Vpwr are connect to 3.0V which…