Other Parts Discussed in Thread: TPS2061 Is it necessary to have an electrolytic on the output? The output of the TPS2061 will power a radio with a 700mA transmit current rating. Can a 22 uF ceramic be used instead of a electrolytic?
Hi Miranda,
Please check TPS2041, TPS2051, TPS2061 and TPS2065, TPS2069
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.…
Part Number: TPS2041C Other Parts Discussed in Thread: TPS2041 , TPS2061 , TPS2513 Hi
I would like to ask about the following application note. That is mentioned about the configuration with a power supply and load switch (such as TPS2041 and TPS2061). …
Hi Anntony,
For TPS2061 is enable is logic low active, when the En-pin lower than 0.8V (VIL) then the device will be active for work. The minimum level for ENX pin to be a "logic high" is 0.8V , it don't depends on Vin voltage . It is OK to contect…
Other Parts Discussed in Thread: TPS2061 Hello,
The TPS2061/2/3/5/6/7 devices are rated at 1A continuous current with a current limit of 1.9A. I am wondering for the two and three channel devices if this applies for each channel. Can each channel provide…
Hello Janice,
Thanks a bunch for the quick response. Our PPATH register settings are performed in u-boot bootloader, and stay intact thereafter. USB WiFi dongle is plugged after complete boot is finalized and we can check and assure that USB current limit…