Part Number: TPS2513A-Q1 Other Parts Discussed in Thread: TPS2513A Dear Ti support Team,
I am working to develop an USB charger with AC using TPS2513A , to detect the charging process from different mobile phones,and your power charger IC,
but we have…
Part Number: TPS2513A Other Parts Discussed in Thread: TPS2513EVM-527 , TPS2513 , TPS2561A , I am using the TPS2513EVM-527 evaluation module to try to charge the battery on the Samsung Galaxy S6 and S3, as well as the iPhone 6S. My input to the evaluation…
Part Number: TPS2513A-Q1 Other Parts Discussed in Thread: TPS2549-Q1 , TPS2513A , TPS254900-Q1 , TPS2514A
Hi,
If TPS2513AQ1 is connected with TPS2549-Q1 as following, can it negotiate about charging mode with USB device correctly ?
I'm supposing that it…
Part Number: TPS2513A-Q1
Hi,
I got following question from my customer.
They would like to know voltage specification of D± which USB device can recognize each modes of charger for their reference.
Could you fill blank of attached file?
Voltage…
Part Number: TPS2513A-Q1
Hi,
My customer is minding variation of D± output voltage by VIN during handshake.
DP DM variation by VIN.xlsx
Could you fill blank of attached files?
It is also no problem similar data.
Best Regards,
Kuramochi
Part Number: TPS2514A Other Parts Discussed in Thread: TPS2513A Hi Sir,
I have question about TPS2514A support mode.
May I know TPS2513A/4A can support 5W/10W/12W? If yes, could you provide test data or recommend it? thanks.
TI TPS2513A/4A D/S show
…
Part Number: TPS2513A-Q1 Other Parts Discussed in Thread: TPS2513A , TPS2549 , TUSB321 Dear support team,
could you please tell me, does TI has Dedicated Charger controller IC, that will support BC 1.2, Apple 2.1A and 2.4A?
I am going to make USB-C charge…
Hi sirs:
My customer have a question that how to set outpur current under 1A .
They change D+/D- connect as followings.
They use iPAD as device, but measure output current over 1A .
Do you have any suggestions for this case?Thank you.
Hi Benny,
Thank you for your answer.
So if I understand:
- with the TPS2513 in 5W mode the maximum negociated current to consume is 1.5A (divider 1 BC1.2)
- with the TPS2513 in 10W mode the maximum negociated current to consume is 2A (divider 2)
-with…