Other Parts Discussed in Thread: TPS2561A , TPS2513A I have a TPS2561A chip and was wondering in which scenario should I get an external power current limiter ?
I'm building a universal usb charger (up to 2A) and my source can draw(have the potential) up…
Steven,
Yes, TPS2513 supports devices from Amazon and Blackberry, the following devices are verified to be work propoerly with TPS2513:
Kindle Fire, Kindle Fire HD.
Blackberry:
7100T
8100 Pearl
8700c Electron
8820 88xx series
8900 Curve
…
Other Parts Discussed in Thread: TPS2513 , TPS2513A Hello,
TPS2513 supports dedicated charging port Auto detect mode, DCP Divider 1(5 W) and Divider 2(10W). TPS2513A supports dedicated charging port Divider mode 3(12W).
My questions are:-
1) I have a…
Other Parts Discussed in Thread: TPS2513 , TPS2513A I'm in the final design stages for a USB charger product that uses your TPS2513 DCP Controller. I just discovered that you now have an "A" version of this part that provides a Divider 3 output to support…
Can you also check the overall topology and all TI component? not only TPS2561A
Is there any better way or component to achieve our design?
We would like our design to be compatible with most device, is TPS2513A suitable?
What's the difference betwee…
Dear teacher,
I have one question for you
since some USB port supports Data+power,for examole, if you plug Cell phone into your computer through USB port, your computer can copy pincutes from your cell phone. But some USB ports only support power (your…
Part Number: TPS254900-Q1 Other Parts Discussed in Thread: TPS2549 , TPS2513A , TPS2514A Hello,
There is not clear shows DCP support in the datasheet, can someone help answer this question?
At the meanwhile, if it cannot support DCP, could I simply connect…
Hi Eric,
Thanks for your answer on "A" device supporting 12W.
May I know, for TPS2513A/TPS2514A, , if we plug in Samsung handphone, what is the maximum charge current it can draw and the mode used?
Best regards,
Gim Song
HI Jory,
Sorry for the delayed response. I had to confirm with the team. For USB Logo certification:
The TPS2511, TPS2513, TPS2513A TPS25213, TPS2414A do no pass as they do not implement VBUS discharge
The TPS2540, TPS2541, TPS2543, and TPS2546 will…