Hi Jared,
While we do not have a ready made reference design to show, your customer could basically use a TPS2513A with one channel supporting BC1.2 charging on the type C port and the other channel supporting BC1.2 on the type A connector. For the type…
Other Parts Discussed in Thread: TPS2511 , TPS2513A , TPS2513 , TPS2561A May I have your help , I learned TPS2511 has some issue especially iPad first plug, if use short timer, the noise of first plug in iPad will trigger TPS2511 from correct Applied divider…
Other Parts Discussed in Thread: TPS2513A Dear Sirs,
Is there anyone know which solution can support new iPad 2.4A charging and compatible with old Apple device charging?
As I know, there are divider 1/2 and divider 3 mode for Battery Charging product…
Other Parts Discussed in Thread: TUSB8040 , TUSB8040A1 , TPS2514A , TPS2513A , TPS2513 , TPS2511 , TPS2514 Hello,
I have question of TUSB8040.
When I use TUSB8040 as DCP only, Is the USB controller not necessary?
When I use TUSB8040 as DCP only, What kind of…
Other Parts Discussed in Thread: TPS2513 , TPS2561 , TPS2511 , TPS2513A My 1 st question is: what benefit(s) are there (or maybe just differences) in implementing a USB charging circuit using the TI parts: TPS2561 and TPS2513 to support a dual USB charger…
Dear Bob,
Thank you for your reply & Sorry for delay in my response.
As I mentioned on my email above, I have tried with 5.5V supply input & Current limit resistor of 20K ( with 5% tol available with me right now, instead of 1%).
Yes, there was…