Part Number: TPS2514A Other Parts Discussed in Thread: TPS2513A Hi Sir,
I have question about TPS2514A support mode.
May I know TPS2513A/4A can support 5W/10W/12W? If yes, could you provide test data or recommend it? thanks.
TI TPS2513A/4A D/S show
…
Other Parts Discussed in Thread: TPS2514 , TPS2514A Hi team,
I have a question about the TPS2514. Can it support Iphone 6S and iphone 6S plus?
My customer uses TPS2514 in usb port but can't charge the iphone7. When they plug in the iphone7, the D+ D- is…
Hi Eric,
Thanks for your answer on "A" device supporting 12W.
May I know, for TPS2513A/TPS2514A, , if we plug in Samsung handphone, what is the maximum charge current it can draw and the mode used?
Best regards,
Gim Song
Hi Adam,
We appreciated your great support!
If customer spec is 5V/1.5A (short D+/D-)for android , 5V/2.4A (D+/D- 2.7V) for Apple.
They want to use TPS2561 A+TPS2514A. could these solution support this case?
They think TPS25810 is too high level.
Could…
Part Number: BQ25883 Other Parts Discussed in Thread: TPS65988 , TPS65987D , TPS2514A Hi,
Why BQ25883 sets the current limit (IINDPM) to 3.0A when he detects DCP charger on the USB? According to the documentation mentions about DCP, the current limit is…
Hello John,
The TPS2514 will work for your desired charging schemes. Divider 1 will charge at 5 W and Divider 2 will charge at 10 W. The voltages applied to the DP/DM are captured below:
The main difference between the TPS2514 and the TPS2514A is the…
Part Number: TPS25740B Other Parts Discussed in Thread: TPS25810 , TPS25740 , TPS25740A , TPS2514A , TPS65987D Hi! I am using TPS25740B for a 5V/3A charger application.
I have a problem with the GDNG pin as it turns on and off. Upon checking the datasheet…
Part Number: TPS25810A-Q1 Other Parts Discussed in Thread: TPS25810-Q1 , , TPS2514A-Q1 Hi,
Except for except for blocks which are different specification as below, are TPS25810A-Q1 chip and TPS25810-Q1 common chip?
e2e.ti.com/.../669445
Best Regards,
K…
Part Number: TPS2511-Q1 Other Parts Discussed in Thread: TPS2549-Q1 , TPS2543-Q1 , TPS2546-Q1 , TPS2514A-Q1 Hi team
I find for MFI certification related USB Conteroller. (Automotive)
Can you recommend me available device?
I found TPS2511-Q1. Another else…