Part Number: BQ25895 Other Parts Discussed in Thread: TPS65988 , , PMP4496 , TUSB320LI , TS3USB221 , TPS2514A Hi everyone ,
I am working a power bank product, and I am already using BQ25895 as PMIC, now I want to upgrade the system to support the USB Type…
Hi Matt,
1) Unfortunately, the TPS25740 does not have dedicated D+/D- pins for Type A connectors applications. This is why on its EVM we use the TPS2514A (separate IC) to handle this.
2) The protocols for D+/D- and the CC lines are not the same. They…
Dear teacher,
I have one question for you
since some USB port supports Data+power,for examole, if you plug Cell phone into your computer through USB port, your computer can copy pincutes from your cell phone. But some USB ports only support power (your…
Part Number: BQ25890H Other Parts Discussed in Thread: BQ25890 , BQ25895 , TPS2514A , TPS2546 Can I use the BQ25890H in OTG mode as a charging device? For example 5V 1,5A. Is it possible to short-circuit the conclusions of D + and D- with BQ25890H? Thank …
Part Number: TPS254900-Q1 Other Parts Discussed in Thread: TPS2514A , TPS2549 Hi,
The TPS254900-Q1 supports short to battery protection for D+/-.
However the TPS254900-Q1 doesn't support Divider3.
If Divider3 and short to battery protection for D+…
Part Number: TPS254900-Q1 Other Parts Discussed in Thread: TPS2549 , TPS2513A , TPS2514A Hello,
There is not clear shows DCP support in the datasheet, can someone help answer this question?
At the meanwhile, if it cannot support DCP, could I simply connect…
Hi, Umberto,
Sorry, we can't find a Samsung S8/S9 to test here.
Our TPS25810 is compliant to type-C standard (pass Ellisys test), it can charge Macbook at 3A advertising speed. In your customer tests, Samsung S8 support type c PD charging doesn…