Hi Srinidhi,
We do not have a device in our portfolio capable of 2 output channels with 2 independent adjustable current limits. This would require 2 single channel switches. I would consider TPS2556, TPS22950x, or TPS25221. There are additional options…
Part Number: TPS2556-Q1 Hi Teams,
Apple carplay asks test 160% times current test for 1ms, how can I pass it?
For example, the charge requirement is 2.1A, so we design the current limit 2.5A which allows low and high limit about 2.2A and 2.7A respectively…
Part Number: TPS2556 Hi Sir,
If the TPS2556 only short-Circuit instant, then how many time Vout power on again?
We are verify on TPS2556DRBEVM-423 is random between 90ms to 170ms,
Does TI have this Range spec?
Hugo
Part Number: TPS2556 The datasheet on the TPS2556DRB only shows 1mm max height. I also need min and typical. I also check the package reference link and the drawing shows no dimensions. www.ti.com/.../mpds118k.pdf
Please forward min and typical height…
Part Number: TPS2556 Hi Expert,
The customer is asking the TPS2556 ESD report.
Pls share the material to us.
Thanks
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
M: +886-909-262-582
E…
Hi KmB,
Sorry, I don't consider this part, yes, you can use the TPS2553, TPS2552D&TPS2553D in the new designs.
If you want the supply current is less than 100uA, how about the TPS2556/7.
Best Regards,
Kuno
Part Number: TUSB1142 Other Parts Discussed in Thread: TUSB321 , , TPS2000E , TPS2001E , TPS2556 , TPS2557 , TUSB320
Hello. As described in a previous post I have to design a board to drive and USB from an USB3 type-C connector to another USB3 connector at…
Part Number: TPS2556 Hi
My customer evaluate TPS2556.
They use 174kΩ as RLIM.
Are there the data about current limit value vs temperature characteristic?
Best regards,
Yokota