Part Number: TPS2557 Other Parts Discussed in Thread: TPS2556 Dear Team,
I have two question regarding "ton" below.
Q1. "ton" turn on delay time is defined as max 9ms according to the datasheet page 6. I can find ton is around 3.8ms…
Part Number: TPS2554 Other Parts Discussed in Thread: TPS2557 , TPS2557DRBEVM-423 Could you pls help check whether TPS2554 have passed UL IEC 62368?
The same for TPS2557.
Could you pls help check whether TPS2557 have passed UL IEC 62368?
Part Number: TPS2557 Hello Team,
I could find that Ternon Time, ton, is 9ms as max under the condition of CL = 1 µF, RL= 100 Ω in the datasheet page 6. Could you let me know the ton under CL=1mF and RL=Open, Vin=3.3V?
Best Regards, Hirokazu…
Part Number: TPS2557 Dear Team,
Does IREV, Reverse leakage current, depends on the condition of EN?
If EN is low and device is disable, will IREV appear at the condition of Vout=6.5, Vin =0V?
Regard,
HirokazuTakahashi
Part Number: TPS2557-Q1 Other Parts Discussed in Thread: TPS25810-Q1 Hi,
Maximum Junction Temperature is specified "internal limited" as below.
Does it mean that this device is not achieved maximum junction temperature because thermal shutdown…
Part Number: TPS2557-Q1 Other Parts Discussed in Thread: TPS25810 , TPS2557
Hi,
How much is the maximum thermal shutdown temperature of TPS2557-Q1?
My customer woud like to know the margin during the maximum thermal shutdown temperature and absolute maximum…
Part Number: TUSB1142 Other Parts Discussed in Thread: TUSB321 , , TPS2000E , TPS2001E , TPS2556 , TPS2557 , TUSB320
Hello. As described in a previous post I have to design a board to drive and USB from an USB3 type-C connector to another USB3 connector at…
Part Number: TPS2557 Dear Team,
We are studying Two-Level Current-Limit Circuit in Figure 22.
Could you let me know the settling time for changing the current limit value at the condition neglecting the slew rate of the external FET Q1?
We want to know…
Part Number: TPS2557 Hi,
What is the probable mode of failure for this device ,. Unit came for repair and It shows "OUT" pin short to ground as well as "IN" pin short to gnd .
Even if the OUT pin is shortcircuited, it is supposed to…