Other Parts Discussed in Thread: TPS2557 Hi all, Please let us know about TPS2557. We have some questions. Questions: - Does this device have a integrate current detection resistor? - If this device has a current detection resistor, how much that the resistance…
Other Parts Discussed in Thread: TPS2557 Hi,
My customer has questions about TPS2557. Could you tell me about questoins?
[Question] - Does the device have internal body diode?
- When EN is Low, it become reverse Input-Output voltage condition. *Vout=6.5V…
Hi all, Please let me know about internal circuit of TPS2557-port. This device is limits the output current by external resistor. Internal circuit of ILIM-port is constant current source? Regard, Yoshi.
Other Parts Discussed in Thread: TPS2557
Hi.
Could you tell me about TPS2557 UL Listed ? Does TPS2557 acquire UL Listed - IEC60950-1-am2?
IEC60950-1-am2 has been released.
Our customer is looking for current limit switch that complies with IEC60950-1-am2…
Other Parts Discussed in Thread: TPS2556 , TPS2557 Dear All,
can yo recommend a load switch that covers Type C 5V 3A with EN and FLT pin?
Like NX5P3363
Best Regards,
David.
Other Parts Discussed in Thread: TPS2557 Greetings... We have an application where we would like to allow bidirectional current flow to/from a power connector. We were considering using twoTPS2557s (or similar). Can two devices be used back-to-back, one…
Part Number: TPS2547 Other Parts Discussed in Thread: TPS2557 Hi team,
I think this is a basic question.
I know some customer uses USB switch such as TPS2557 in USB host for charging USB device. Charging port controller such as TPS2547 looks like more…
I have question of current protection accuracy by temp.
An expression of "Iosmax Iostyp Iosmin" is written on datasheet p11 .
Are these expresions included in the accuracy by the temperature?
Other Parts Discussed in Thread: TPS2557 Hello, My name is Hidetoshi Matsunami.
I would like to ask you about the limit of output capacitance for TPS2557.
What is the limit value of output capacitance?
I'm concerned this device is in danger of breaking…
Other Parts Discussed in Thread: TPS2557 Hello, I am using TPS2557. I set Iosnom to 3.5A using Rilim=31.6kohm. When the load current is 3.5A, OUT-terminal remains High though FAULT-terminal is Low.
Is this function correct? Does this phenomenon occur between…