Other Parts Discussed in Thread: TPS2557 Hello, I am using TPS2557. I set Iosnom to 3.5A using Rilim=31.6kohm. When the load current is 3.5A, OUT-terminal remains High though FAULT-terminal is Low.
Is this function correct? Does this phenomenon occur between…
Other Parts Discussed in Thread: TPS2066 , TPS2065 , TPS2557 Hello sir
We have customer which plan to use TPS2557 ,TPS2066 ,TPS2065.
And Customer ask CB TEST Data of each devices when they would like to launch their new Production now.
How can we get CB TEST…
Other Parts Discussed in Thread: TPS2557 Hi, I have a question regarding maximum current into the fault pin on TPS2557.
In the datasheet, you state an absolute maximum continuous current of 25mA, but there is no information about maximum peak current.…
Part Number: TPS2042B Other Parts Discussed in Thread: TPS2556 , TPS2066 , TPS2064 , TPS2560 , TPS2052 , TPS2557 Hi Team,
a customer asks if there is a suitable alternative for the TPS2042BDR. (preferably p2p)
Thanks and regards
Roman
Hi Zirui,
Don't have p2p device. But have similar function device, such as TPS2556-Q1 and TPS2557-Q1.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help…
Part Number: TPS2559 Other Parts Discussed in Thread: TPS2557 , TPS25221 Dear Team,
The customer is interested in TPS2559, do we have a more competitive device to replace TPS2559?
Do you have a comparison table to compare TPS2559 and TPS2557, appreciated…
Part Number: TPS2557 Dear Sir/Madam,
I would like to check with you on resister value using at EN pin and FAULT pin.
Based on IC specification is using 100Kohm but EVM using 10Kohm
Circuit from IC specification.(using 100Kohm)
Circuit from EVM…
Part Number: TPS2561 Other Parts Discussed in Thread: TPS2557
Hi team,
I want to use TPS2561 as a current limited power switch and can auto retry, there is no battery in the schematic, there are some DC/DC and MCU in the schematic. The USB port connect…
Part Number: TPS2511 Other Parts Discussed in Thread: TPS2549 , TPS2513 , TPS2561 , TPS2557 I have a design that I would like to decrease the RdsON that I am getting with the current part, a TPS2511.
I have looked at a TPS2549 but it does not seem to have…