Part Number: TPS25740B I have a doubt in configuring the TPS25740BEVM-741 . it has two connectors, J7 and J8 for HIPWR and PCTRL configuration. I didn't understand which of those pins to connect to configure it to P1 and H1. Kindly help me config…
Part Number: UCC28780 Other Parts Discussed in Thread: UCC24612 , , TPS25740B
Dear,
our client use UCC28780 and UCC24612 and TPS25740B for 65W Type-C Application
Could help me suggestion schematic and layout as below file.
schematic:
Transformer design information…
Part Number: TPS25740B Other Parts Discussed in Thread: LM5175 , TPS25740 Hi!
I have built PCB based on TPS25740B-741 Evaluation Module.
Problem I am facing is that if I apply load on Type-C port TPS25740B is disconnecting output and falling back to 5V.…
Part Number: TPS25740B Other Parts Discussed in Thread: TPS2421-2 When I transition down from any voltage to any voltage, it all works great, except the +15V -> +5V.
When transitioning DOWN from one voltage to another, the TPS25740B turns ON a discharge…
Part Number: TPS25740B Other Parts Discussed in Thread: TPS65982 , TPS65981 Hello,
I'm designing a charging station for a customer. My customer would like use an off the shelf USB Type C wall charger as the power source. The sink would be charging contacts…
Part Number: TPS25740B Hi Team, The datasheet shows the following and I believe TPS25740B is intended to use for an application that doesn't support USB data communication. Is my understanding correct? Best Regards, Yaita
Other Parts Discussed in Thread: TPD4E05U06-Q1 , TPD1E01B04-Q1 , TPD1E05U06-Q1 , TPD1E10B06-Q1 , TPD1E05U06 , TPS25740B Hello,
I am searching the ESD Protection Device for Type-C' s CCx, DM and DP pins.
I wonder what is the nominal working voltage of these…
Other Parts Discussed in Thread: TPS65987D , TPS25740B Hello,
I am working on a project that involves USB ports for aircrafts. Do you have any new switch-mode power supply devices that take 115VAC down to a the newer USB Type-C specifications where the…
Hello, The schematic is available within the user's guide. However, we do not recommend incorporating the TPS25740B into future projects, but instead the TPS65987D.