Hi Donovan,
We are applying for sample of TPS25740B.
I have a question about TPS25740B : There is the same deglitch time of 120us described in the datasheet of TPS25740 and TPS25740B,is the datasheet of TPS25740B not updated ?
How long is the deglitch…
Part Number: TPS25740 Hello TI engineer,
right now I want buy TPS25740B to build a board(usb-pd+flyback) for type-c application, when I purchase it on mouser, found there are a lot of part number, such as TPS25740BRGER , TPS25740BRGE T, TPS25740ARGER , TPS2…
Part Number: PMP40312 Other Parts Discussed in Thread: TPS25740B , Hi Team,
I am designing a 100W PD car charger solution.
Can you suggest a car charger IC, that can handle 100W(20V,5A)?
Although, I have seen 100W PD controller IC----TPS25740. ( www.ti.com…
Other Parts Discussed in Thread: TPS25740B Hi
Does TI have Type C PD solution that can support PPS certified ? applicaiton is adaptor. I see TPS25740B can support PD3.0, but it can not adjust output voltage by 20mV steps, it's fixed 4point output voltage…
Part Number: TPS25740A Other Parts Discussed in Thread: TPS25740B , Hi Team,
I see the TID# in the TPS25740B datasheet, what is the number for the A version?
Thank you!
Regards,
~John
Hi Garrett,
Thanks for responding so quickly. I only discovered this by chance when putting a TPS25740BEVM through some tests. The current was measured at the supply ( VIN ) and this was not changed. What did change, was the LM5175 deciding to either…
Hi Rocson,
As Donovan pointed out, there has been some talk on the matter of getting the TPS25740B automotive qualified. However, it is still at it's infancy stage with no definite timeline.
The TPS25740B is P2P with the TPS25740. Both devices…
Hello,
Consider checking out the TPS25740B for your application. It is a simple DFP PD Controller that supports 5V, 9V, 15V, and 20V output voltages.
If this answers your question, PLEASE select This resolved my issue
Thank you,
Eric
Hi Saranya,
You are on the right track with the TPS25740B since this device is mostly used in chargers and power banks.The USB DFP controller(TPS25740B) has two voltage settings 5V,9V,15V,20V and 5V,9V,12V,15V that are fixed based on a voltage divider…