Part Number: TPS25820 Hi TI,
I'm using the TPS25820DSST device in my system, communicating the /SINK and /FAULT status to a processor elsewhere in the board. Per the datasheet's recommendation, those lines are pulled-up via seperate 100kohm resistors…
Part Number: TPS25820 Other Parts Discussed in Thread: HD3SS3202 I'm HW engineer from BOE, and used TPS25820 (PD controller) and HD3SS3202 (USB3.1 MUX/DEMUX) for the USB-C mater port supporting 1.5A PD power source. The project is a video conference display…
Part Number: TPS25820 Other Parts Discussed in Thread: TUSB1142 , TUSB320 Dear TI Forum,
is it possible to use the TPS25820 together with the TUSB1142 similar to the EVM,
but I would like to use it in an endpoint device.
Does it work by just adding…
Part Number: TPS25820 Tool/software: Hi team,
I am confuse the below list in TPS25820 datasheet: When various type-c port, Why CC1 and CC2 have various status? Where Ra and Rd comes from ?
BR
Amber
Part Number: TPS25820 Tool/software: Hi,
The customer circuit design is as follows, but only about 900m output current, measured whether the CHG end is 5V high level, not connected to 100k direct pull-up test, or only 900mA output.
Please help to…
Part Number: TPS25820 Other Parts Discussed in Thread: TPS25751
Tool/software:
I'm trying to get the TPS25820 to work as a USB Hub PD controller. I want to supply 1.5A output current to charge the attached cell phone, while allowing the cell phone…
Other Parts Discussed in Thread: TPS25820 Hello,
Using TPS25820 & Type C to Type C connection, I want to understand the current limit after attach as per USB PD3.2. In USB2.0, it is 100mA before enumeration. Does same apply here ?
Part Number: TPS25820 Tool/software: Hi,
I am developing a smart cable and found that TPS25820 is a good choice. However, from the datasheet I couldn't find detailed design guide lines for using the VCONN feature. Of course it is all according to the…
Part Number: TPS25820 I have created a design using a TPS25820 with a USB-C connection. As I was reading through the data sheet I noticed on page 19 of the data sheet the following:
" However with DCP implementation the port will not support any data…
Part Number: TPS25820 hi Teams:
Please help review the schematic diagram below. Thank you.
1. The input is USB-A and the output is USB-C. Now, it is required that the output USB-C has no power when not connected to Device, and only when connected…